Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MBCC breakout carrier board problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 662 views
  • Users 0 members are here
Related

MBCC breakout carrier board problem

xzsawq21
xzsawq21 over 8 years ago

Hello

I have checked the MBCC Breakout carrier board's datasheet for MicroZed. I see a problem!

we can calculate the output voltage for the LMR10510 as follow:

Vout=0.6*(1+R1/R2)

you can find above folrmula at page 12 of the below datasheet:

http://www.ti.com/lit/ds/symlink/lmr10510.pdf

 

but in your design:

http://s8.picofile.com/file/8316564600/LMR10.JPG

image

 

as your design to produce 2.5V we have:

Vout=0.6(1+107k/10k)=7.02 !!!

could you please clear this problem?

for other output voltage there is the same problem.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 8 years ago +1 verified
    Hello Xzsawq21, Excellent question! If you refer to the schematic you will notice that the 45.3k Ohm resistor is shorted. This is done so when no Jumper is placed 3.3V VADJ is present by default. So when…
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Xzsawq21,

    Excellent question! If you refer to the schematic you will notice that the 45.3k Ohm resistor is shorted. This is done so when no Jumper is placed 3.3V VADJ is present by default.

    image

     

    So when jumper position is 3-4 is placed you have a 107k and a 45.3k Ohm resistor placed in parrallel. So to find the resistance of the parrallel resistors you do 1/(1/107k+1/45.3k) = 31.82k Ohm.

    Now we plug that into the forumla from the TI datasheet you provided we get

    Vout = .6(1+31.82k/10k) = 2.509V which is correct.

    This is similar to how the 1.8V VADJ was calculated.

     

    Let me know if you need a further explination.

     

    Thanks,

    Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Xzsawq21,

    Excellent question! If you refer to the schematic you will notice that the 45.3k Ohm resistor is shorted. This is done so when no Jumper is placed 3.3V VADJ is present by default.

    image

     

    So when jumper position is 3-4 is placed you have a 107k and a 45.3k Ohm resistor placed in parrallel. So to find the resistance of the parrallel resistors you do 1/(1/107k+1/45.3k) = 31.82k Ohm.

    Now we plug that into the forumla from the TI datasheet you provided we get

    Vout = .6(1+31.82k/10k) = 2.509V which is correct.

    This is similar to how the 1.8V VADJ was calculated.

     

    Let me know if you need a further explination.

     

    Thanks,

    Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer