Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design 12V Supply vs. 5V
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 342 subscribers
  • Views 389 views
  • Users 0 members are here
Related

12V Supply vs. 5V

Former Member
Former Member over 10 years ago

Hey,

I have a short question. I want to build a Carrier Card for the MicroZed and I read that I can use for supply voltage 12V or 5V. And I also read that the MicroZed have with 12V an higher power consumption.

So my question is, using 5V(from the u00B5Headers) instead of 12V do I loose computing power on the chip? Or is there a different mode if I'm using 12V? Or what I'am losing if I take 5V?

I use the board with the 7020 Zynq.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Hello Christian,

     

    You can use a supply voltage of 12 V for the MicroZed, but it does require some modifications to the MicroZed as outlined in section 2.10.2 of the MicroZed Users Guide:

     http://microzed.org/sites/default/files/documentations/MicroZed_HW_UG_v1_6.pdf

     

    You will also  need to reference the MicroZed schematic:

     http://microzed.org/sites/default/files/documentations/MicroZed_Rev_F_Schematic_141212.pdf

     

    The only additional power consumption should be from the addition of the regulator dropping the 12V input to 5V. Otherwise the operation of the MicroZed should be identical, with no reduction in computing power.

     

    You can also request a quote for customized MicroZed SOMs with the 12V modifications made at the factory. Contact your local Avnet / Silica FAE for details, or you can contact customize@avnet.com if you do not know your local FAE.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Hello Gary,

    thanks for your answer!

    That should be the reason for the higher power consumption.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    As per my experience you can use a supply voltage of 12 V for the MicroZed, but it does require some modifications to the MicroZed.
    The only additional power consumption should be from the addition of the regulator dropping the 12V input to 5V.
    Otherwise the operation of the MicroZed should be identical, with no reduction in computing power.