Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed XADC pins + Connections BKO Carrier
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 570 views
  • Users 0 members are here
Related

Microzed XADC pins + Connections BKO Carrier

lucileklang
lucileklang over 9 years ago

Hello !

I'm trying to use the XADC on the Microzed 7010 to input analog signal and filter it on the FPGA. I have a Breakout Carrier Card to enable this analog input.

I looked at the pins that connect the VP_0_P and the VN_0_N to the JX1 microheader :
(http://microzed.org/sites/default/files/documentations/MicroZed_HW_UG_v1_4.pdf   page 18)

VP_0_P : Bank 0, L10     JX1Pin : 97

VN_0_N : Bank 0, K9      JX1Pin : 99

Then I took a look at the BKO card to see where to connect my input signal. I searched for the JX1Pin 97 and 99, but they both are referenced as GND.

(http://zedboard.org/sites/default/files/documentations/5271-UG-MBCC-BKO-V1.2.pdf   page 10)

Thus I'm confused to where I should connect my inputs to use the dedicated Vp and Vn inputs of the SoC.

Any help would be greatly appreciated, thank you !

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Luc,

    If you look in the BKO card HW User Guide, section 2.1.3. it states Bank 35 exposes several I/Os that may be used as analog inputs to the XADC.

     

    You could try looking into bank 35 for the application you wish to run.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hello Luc,

    you can use the ADC channel 0 out of xadc 8 channels connected to connecter2 of breakout board.

    CON2, pin 5 IO_L1P_T0_35 JX2, pin 17 Bank 35, C20 IO_L1P_T0_AD0P_35
    CON2, pin 7 IO_L1N_T0_35  JX2, pin 19 Bank 35, B20 IO_L1N_T0_AD0N_35
     
    pin 7 n channel must be grounded for propper readout if you are using single ended signal.
    Thanks