Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed PMOD Zynq PS MIO I2C controller registers unmapped
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 2416 views
  • Users 0 members are here
Related

MicroZed PMOD Zynq PS MIO I2C controller registers unmapped

jamestkennedy
jamestkennedy over 9 years ago

The design uses Petalinux OpenAMP primarily as a data engine using the Ethernet port to process data and deliver to the microheader. So the MicroZed is a daughter card on a custom PCB that receives the processed data.

However we are also attempting to use the PMOD to connect to an I2C and a GPIO device.

The standard driver for the Zynq PS I2C controller under PetaLinux is Cadence I2C_cadence which operates the PS I2C controller through its registers.

Well the user level /dev/i2c0 writes were not working, so I added a custom module with the i2c_cadence as the basis and connected it to the I2C0 controller in the device tree to see how the driver was failing.

What I found using debug trace is that the I2C controller registers are not connected to their specified address 0xE0004000. Somehow its addresses on the IOP are not mapped. Regardless of what is written all the R/W registers read 0, and obviously the I2C controller function was not being executed.

Other peripherals on the IOP range of addesses UART, ENET work fine.

I am using Vivado 2016.2 and Petalinux 2016.2. The I2C0 is selected on MIO 14, 15 for SCL and SDA respectively, and the device tree specifies the normal 0xE0004000 as the register address for the controller.

Has anyone encountered this and found their mistake? Or any other suggestions?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi James,

    Correct me if I am wrong, but I assume that you are adding one or more slave devices to MicroZed via the PS Pmod and that this is not a multi-master configuration.

    If this case, the recommended approach would be to use the Cadence driver and register I2C slave devices under it within the device tree.  Once they are registered, then the slave device drivers can be used to communicate with the slaves and the cadence driver then becomes mostly transparent for you.

    In your top level DTS all of the lower level dtsi files can be overridden with additional parameters.  In the top level DTS (where the status = "okay" is found) that is where you should start adding definitions for each of the slave devices.

    Here is an example device tree entry from one of the reference designs for our MicroZed EMBV which also uses PS I2C controller:

    &i2c0 {

         status = "okay";

        

         i2cswitch@70 {

               compatible = "nxp,pca9548";

               #address-cells = <1>;

               #size-cells = <0>;

               reg = <0x70>;

     

               i2c@0 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <0>;

                    pca9354_0: gpio@20 {

                         compatible = "nxp,pca9534";

                         reg = <0x20>;

                         gpio-controller;

                         #gpio-cells = <2>;

                         /*

                         gpio_hdmii_reset_b {

                               gpio-hog;

                               gpios = <0 1>;

                               output-high;

                         };

                         */

                    };

               };

     

               i2c@1 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <1>;

                    adv7611: hdmi-rx@4c {

                         compatible = "adi,adv7611";

                         reg = <0x4c>;

     

                         reset-gpios = <&pca9354_0 0 1>;

                         hpd-gpios = <&pca9354_0 2 0>;

     

                         adi,default-input = <0>;

     

                         #address-cells = <1>;

                         #size-cells = <0>;

     

                         port@0 {

                               reg = <0>;

                         };

                         port@1 {

                               reg = <1>;

                               embv_adv7611_out: endpoint {

                                    remote-endpoint = <&embv_vcap_hdmi_in>;

                               };

                         };

                    };

               };

              

               i2c@2 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <2>;

                    embv_adv7511: adv7511@39 {

                         compatible = "adi,adv7511";

                         reg = <0x39>;

                        

                         pd-gpios = <&pca9354_0 4 0>;

                        

                         adi,input-depth = <8>;

                         adi,input-colorspace = "yuv422";

                         adi,input-clock = "1x";

                         adi,input-style = <2>;

                         adi,input-justification = "left";

                         adi,clock-delay = <0x06>;

                         adi,embedded-sync = "true";

                        

                    };

               };

               /*

               i2c@4 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <4>;

                    adau1761: adau1761@3b {

                         compatible = "adi,adau1761";

                         reg = <0x3b>;

                    };

               };

               */

               /* PYTHON-1300-C camera module */

               i2c@5 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <5>;

                    /* prototype hardware : PCA9554 at address 0x3C */

                    /*

                    pca9554_0: gpio@3c {

                          compatible = "nxp,pca9554";

                         reg = <0x3c>;

                         gpio-controller;

                         #gpio-cells = <2>;

                    };

                    */

                    /* production hardware : PCA9554 at address 0x24 */

                    pca9554_0: gpio@24 {

                         compatible = "nxp,pca9554";

                         reg = <0x24>;

                         gpio-controller;

                          #gpio-cells = <2>;

                    };

               };

         };

     

    From this MZEMBV specific mzembv-top-sdsoc.dts file, we can see that the following devices are being controlled by the above PS I2C driver:

    •   PCA9548 (I2C mux)
    •   PCA9534 (I2C I/O expander)
    •   ADV7611 (HDMI input)
    •   ADV7511 (HDMI output)
    •   PCA9554 (I2C I/O expander, on PYTHON camera module)

    My recommendation would be to use one of those slave device drivers as an example starting point for the I2C slave device you are prototyping up right now.  Again, this is all assuming that you are using a single master to multiple slave I2C bus architecture.

     

    Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 9 years ago

    Hi James,

    Correct me if I am wrong, but I assume that you are adding one or more slave devices to MicroZed via the PS Pmod and that this is not a multi-master configuration.

    If this case, the recommended approach would be to use the Cadence driver and register I2C slave devices under it within the device tree.  Once they are registered, then the slave device drivers can be used to communicate with the slaves and the cadence driver then becomes mostly transparent for you.

    In your top level DTS all of the lower level dtsi files can be overridden with additional parameters.  In the top level DTS (where the status = "okay" is found) that is where you should start adding definitions for each of the slave devices.

    Here is an example device tree entry from one of the reference designs for our MicroZed EMBV which also uses PS I2C controller:

    &i2c0 {

         status = "okay";

        

         i2cswitch@70 {

               compatible = "nxp,pca9548";

               #address-cells = <1>;

               #size-cells = <0>;

               reg = <0x70>;

     

               i2c@0 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <0>;

                    pca9354_0: gpio@20 {

                         compatible = "nxp,pca9534";

                         reg = <0x20>;

                         gpio-controller;

                         #gpio-cells = <2>;

                         /*

                         gpio_hdmii_reset_b {

                               gpio-hog;

                               gpios = <0 1>;

                               output-high;

                         };

                         */

                    };

               };

     

               i2c@1 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <1>;

                    adv7611: hdmi-rx@4c {

                         compatible = "adi,adv7611";

                         reg = <0x4c>;

     

                         reset-gpios = <&pca9354_0 0 1>;

                         hpd-gpios = <&pca9354_0 2 0>;

     

                         adi,default-input = <0>;

     

                         #address-cells = <1>;

                         #size-cells = <0>;

     

                         port@0 {

                               reg = <0>;

                         };

                         port@1 {

                               reg = <1>;

                               embv_adv7611_out: endpoint {

                                    remote-endpoint = <&embv_vcap_hdmi_in>;

                               };

                         };

                    };

               };

              

               i2c@2 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <2>;

                    embv_adv7511: adv7511@39 {

                         compatible = "adi,adv7511";

                         reg = <0x39>;

                        

                         pd-gpios = <&pca9354_0 4 0>;

                        

                         adi,input-depth = <8>;

                         adi,input-colorspace = "yuv422";

                         adi,input-clock = "1x";

                         adi,input-style = <2>;

                         adi,input-justification = "left";

                         adi,clock-delay = <0x06>;

                         adi,embedded-sync = "true";

                        

                    };

               };

               /*

               i2c@4 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <4>;

                    adau1761: adau1761@3b {

                         compatible = "adi,adau1761";

                         reg = <0x3b>;

                    };

               };

               */

               /* PYTHON-1300-C camera module */

               i2c@5 {

                    #address-cells = <1>;

                    #size-cells = <0>;

                    reg = <5>;

                    /* prototype hardware : PCA9554 at address 0x3C */

                    /*

                    pca9554_0: gpio@3c {

                          compatible = "nxp,pca9554";

                         reg = <0x3c>;

                         gpio-controller;

                         #gpio-cells = <2>;

                    };

                    */

                    /* production hardware : PCA9554 at address 0x24 */

                    pca9554_0: gpio@24 {

                         compatible = "nxp,pca9554";

                         reg = <0x24>;

                         gpio-controller;

                          #gpio-cells = <2>;

                    };

               };

         };

     

    From this MZEMBV specific mzembv-top-sdsoc.dts file, we can see that the following devices are being controlled by the above PS I2C driver:

    •   PCA9548 (I2C mux)
    •   PCA9534 (I2C I/O expander)
    •   ADV7611 (HDMI input)
    •   ADV7511 (HDMI output)
    •   PCA9554 (I2C I/O expander, on PYTHON camera module)

    My recommendation would be to use one of those slave device drivers as an example starting point for the I2C slave device you are prototyping up right now.  Again, this is all assuming that you are using a single master to multiple slave I2C bus architecture.

     

    Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jamestkennedy
    0 jamestkennedy over 9 years ago in reply to zedhed

    Hi Kevin,

    Thanks again for your help. I really appreciate it.

    Actually there is only one I2C slave device attached to the PMOD. I tried the DTS approach with a slave that you describe, without effect.

    In the ZedBoard I had used the PL based axi_iic core as I2C0, but just used the dev-i2c0 to access it, so I used the same approach under Petalinux and the generated DTS and DTSI sustained this configuration.

    For this EEPROM fixture, I did encounter a problem where the driver missed the end of send interrupt, so I modified it to use a poll on the isr status register to complete the message process.

    So I presumed that I may be encountering a similar problem here on the MicroZed SOM. But what I found was not the case. I don't see anything in your reply that would lead to thining that the DTSI is superseding the 0xe0004000 address for the bank of registers. And I don't see anything in my design. But the kernel debug trace revealed that the registers somehow were not actually mapped and writing to the register address was like to a floating memory address. The written data for R/W registers did not read back.

    I can't find anything in the design whether Vivado or Petalinux in the device tree that would lead to this failure to map the addresses. The driver sees the 0xe0004000 and does the IO resource remap, but obviously it doesn't work.

    I guess this part of the design will remain TBD until the main board is available.

    BTW, what they asked also is to look into using the same PMOD with 2 devices attached. I.E., with the I2c on 4 Pmod pins of the bottom row  pins 7-12  and a gpio on the top row 0-6, using the appropriate MIO to connect to the PS controllers, but I hadn't even gotten to testing this. When I looked at the GPIO alone under sysfs I was unable to effect a change in the 0/1 status of the inputs. Again as if the register ports were not mapped. Do you think there is some Linux .config setting that I am missing?

    But thanks for trying. If something occurs to me I will be sure to post

     

    Sincerely,

    James