Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed PMOD Zynq PS MIO I2C controller registers unmapped
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 2416 views
  • Users 0 members are here
Related

MicroZed PMOD Zynq PS MIO I2C controller registers unmapped

jamestkennedy
jamestkennedy over 9 years ago

The design uses Petalinux OpenAMP primarily as a data engine using the Ethernet port to process data and deliver to the microheader. So the MicroZed is a daughter card on a custom PCB that receives the processed data.

However we are also attempting to use the PMOD to connect to an I2C and a GPIO device.

The standard driver for the Zynq PS I2C controller under PetaLinux is Cadence I2C_cadence which operates the PS I2C controller through its registers.

Well the user level /dev/i2c0 writes were not working, so I added a custom module with the i2c_cadence as the basis and connected it to the I2C0 controller in the device tree to see how the driver was failing.

What I found using debug trace is that the I2C controller registers are not connected to their specified address 0xE0004000. Somehow its addresses on the IOP are not mapped. Regardless of what is written all the R/W registers read 0, and obviously the I2C controller function was not being executed.

Other peripherals on the IOP range of addesses UART, ENET work fine.

I am using Vivado 2016.2 and Petalinux 2016.2. The I2C0 is selected on MIO 14, 15 for SCL and SDA respectively, and the device tree specifies the normal 0xE0004000 as the register address for the controller.

Has anyone encountered this and found their mistake? Or any other suggestions?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I may have encountered the same problem with the I2C controller. I am using the I2C c

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I may have encountered the same problem with the I2C controller. I am using the I2C c