Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design AXI Address width error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 360 subscribers
  • Views 195 views
  • Users 0 members are here
Related

AXI Address width error

e14 Contributor
e14 Contributor over 12 years ago

I set up the AXI slave with 32 registers.  As my design got further along I discovered I needed 40 registers.  So in an attempt to add to the address width I opened the wizard in IP customization Parameters tab.  I double clicked on the AXI address.  I could see it was set to 7 as the maximum so I closed it.  Now I get an error [IP_Flow 19-345] User Parameter 'C_S00_AXI_ADDR_WIDTH': Default value 7 is greater than the validation maximum 0
The local address width is still 4 for 32 registers and I cannot get rid of the error.