Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed I2C for PMOD Trouble
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 362 subscribers
  • Views 786 views
  • Users 0 members are here
Related

MicroZed I2C for PMOD Trouble

e14 Contributor
e14 Contributor over 12 years ago

I have successfully used I2C on a ZC706 but I find I'm really struggling to troubleshoot the I2C on the MicroZed.

The process seems like it should be simple.  I created a block design that simply contains a Zynq and turns on the I2C 0 and assigns it to MIO 14 + 15 (pins 9 + 10 on J5).

I'm trying to access it from Linux, and when I run a command like i2cdetect, I don't even see the clock on the any of the J5 pins when using an oscilloscope.  Also, if I enable the pullup on those lines, I still don't see any of the pins being pulled high.

Is anyone succesfully using and I2C PMOD on J5 and able to point me in the right direction?

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I was not updating the FSBL for the new design.  With an updated FSBL everything was fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bkamen
    0 bkamen over 11 years ago in reply to e14 Contributor

    What did you do to do this?

    I tried the "petalinux-config --get-hw-description=<path to my project.sdk>" and it doesn't seem to work. Or at least I'm not sure.

    I've scoped the signals and while I have in my Vivado project the SCL/SDA lines config'd with PULLUPS, the voltages on the line are 0 and not Vdd.

    Thanks,

    -Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bkamen
    0 bkamen over 11 years ago in reply to bkamen

    nevermind -- it seems the command previously listed wasn't doing something right to update the FSBL.

    I saved out my changes to system-top.dts and then nuked the directory and re-created the project from scratch -- THEN it worked.

    So something with the bootloader build scripts is messed up.

    (this was with Petalinux 2014.2)

    Yay -- more bugs.

    -Ben