Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design microzed z020 and I/o Carrier card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 322 views
  • Users 0 members are here
Related

microzed z020 and I/o Carrier card

e14 Contributor
e14 Contributor over 12 years ago

Hi
I could not find the pin details for z020 microheader to the peripherals on the I/O carrier card.
Can you please point me to where this documentation is?

I downloaded the IOCC design.zip to  look for the pin outs but those are for z010 , I need for the z020

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In the section 2.8.2 on the MicroHeaders in the MicroZed Hardware Users Guide it discusses the fact that only the 7020 device supports Bank 13. Table 11 in the MicroZed Hardware Users Guide notes that the eight Bank 13 pins on JX1 and the seven Bank 13 pins on JX2 are only available on the 7020 version of the MicroZed.

     

    So the I/O listed in Table 12 (JX1) and Table 13 (JX2) as Bank 13 are the additional signals available with the 7020 device. These IO also have a different power rail, Vcco_13 (JX2-98).

     

    This is also detailed in the MicroZed Carrier Design Guide and in the individual Carrier Card Hardware Users Guides.

     

    The MicroZed Hardware Users Guide and the MicroZed Carrier Design Guide can be found here: http://www.microzed.org/support/documentation/1519

     

    The MicroZed IOCC Hardware Users Guide is here: http://www.microzed.org/support/documentation/1522

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In the section 2.8.2 on the MicroHeaders in the MicroZed Hardware Users Guide it discusses the fact that only the 7020 device supports Bank 13. Table 11 in the MicroZed Hardware Users Guide notes that the eight Bank 13 pins on JX1 and the seven Bank 13 pins on JX2 are only available on the 7020 version of the MicroZed.

     

    So the I/O listed in Table 12 (JX1) and Table 13 (JX2) as Bank 13 are the additional signals available with the 7020 device. These IO also have a different power rail, Vcco_13 (JX2-98).

     

    This is also detailed in the MicroZed Carrier Design Guide and in the individual Carrier Card Hardware Users Guides.

     

    The MicroZed Hardware Users Guide and the MicroZed Carrier Design Guide can be found here: http://www.microzed.org/support/documentation/1519

     

    The MicroZed IOCC Hardware Users Guide is here: http://www.microzed.org/support/documentation/1522

     

    -Gary