Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Boot Error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 508 views
  • Users 0 members are here
Related

Microzed Boot Error

e14 Contributor
e14 Contributor over 11 years ago

Hi all,
I followed the xilinx tutorial. However when I boot the sdcard I get.

*******************************************
U-Boot 2013.01-dirty (Jun 14 2013 - 16:25:48)
DRAM:  512 MiB
WARNING: Caches not enabled
MMC:   zynq_sdhci: 0
SF: Detected S25FL129P_64K with page size 64 KiB, total 16 MiB
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Controller never released inhibit bit(s).
Device: zynq_sdhci
Manufacturer ID: 2
OEM: 544d
Name: SA04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 1-bit
Loading bitstream from SD/MMC/eMMC to RAM..
Controller never released inhibit bit(s).
Device: zynq_sdhci
Manufacturer ID: 2
OEM: 544d
Name: SA04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 1-bit
Controller never released inhibit bit(s).
** Bad device mmc 0 **
***************************************

I tried many way but it didn't work. What am I missing??
Boot.bin: command build <bootgen -image boot.bif -o i boot.bin>
Thanks in advance for any advice you can give me.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Could you be a little more specific on which Xilinx tutorial you are following? Does it target the MicroZed or a Xilinx evaluation board?

     

    What type of MicroZed do you have? What host operating system are you using?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I was following this tutorial(http://www.wiki.xilinx.com/Prepare+boot+image). My's target is Microzed. I am using Microzed Rev.C(http://zedboard.org/product/microzed). Host opreating system is WinXP. Xilinx tool version 14.5.

    Be

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I was solved my's problem. Thanks TroutChaser.