Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Program FPGA failed when FMC (DC1532A-L) plugged into FMC-Carrier Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 362 subscribers
  • Views 3041 views
  • Users 0 members are here
Related

Program FPGA failed when FMC (DC1532A-L) plugged into FMC-Carrier Card

nowksru
nowksru over 8 years ago

Hello,

I am trying to program the MicroZed through the FMC-Carrier Card via JTAG, while the FMC module DC1532A-L (Linear Technology) is plugged in the Carrier Card. But when I click on the Program FPGA button in Xilinx SDK (2017.4) I get the following error message:

"Could not find FPGA device on the board for connection 'Local'.

Troubleshooting hints:
1. Check whether board is connected to system properly.
1. In case of zynq board, check whether Digilent/Xilinx cable switch settings are correct.
1. If you are using Xilinx Platform Cable USB, ensure that status LED is green.
Program FPGA failed"

If I unplug the FMC module from the Carrier Card, SDK runs the programming without a problem --> board is connected to system properly and status LED is green in both cases (FMC module plugged in & unplugged). I guess the FMC module is somehow interfering with the JTAG pins?
 

I don't know if it is important, but my application is just reading registers on the FMC module through SPI.
 

-Urs


 

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 8 years ago +1
    Hi Urs, I believe your right. This makes sense. As far as the best way to tie these pins together. My suggestion would be to break out your soldering iron and modify the MicroZed FMC Carrier Card. Looking…
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi Urs,

    did you verify the pinout matched up between the MZ fmc and the Fmc your plugging in?

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi Urs,

    did you verify the pinout matched up between the MZ fmc and the Fmc your plugging in?

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hi Josh,

    I checked all the connected pins on the module and they match the FMC-CC. Two things are noticable, that is the JTAG pins (TCK, TDI, TDO, TMS) on the FMC connector of the module are not connected. I have seen a document of another module, where the manufacturer short-circuited TDO and TDI, as it is mentioned in this document of the ANSI/VITA57 standard: "[...]if JTAG chain is not used by mezzanine card, short TDI and TDO."

    The other thing is that LA01_P_CC (cc stands for clock capable pin) is shorted to LA05_P and LA01_N_CC is shorted to LA05_N. I don't see a problem here, although I have no idea why they did these short-circuits.

    -Urs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hi Josh,

    it looks like I have to short TDI and TDO (on the FMC connector) or somehow bypass the JTAG connection on the FMC connector in order to sustain the JTAG chain as it solved other peoples problems, which seem similar:

    http://zedboard.org/content/error-scanning-jtag-chain

    https://forums.xilinx.com/t5/Evaluation-Boards/ZC706-FMC-Connector-JTAG-Bypass/td-p/400829

    http://zedboard.org/content/jtag-breaks-using-fmc-dac

    Do you have any idea on how to do this with the FMC Carrier Card as there is no jumper or switch for this at present?

    Thanks

    -Urs