Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design unused pins
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 527 views
  • Users 0 members are here
Related

unused pins

e14 Contributor
e14 Contributor over 10 years ago

Hello,

 

In my custom carrier card design I will leave several pins without using and I was wondering how to connect those pins: floating or grounding. Most of the pins are dedicated for signals but others are connected to specific nets which I have left floating according to the recommendations: 4 JTAG, CARRIER SRST, FPGA DONE, FPGA VBAT, 8 PMOD and INIT.

On the other hand, I also wondered whether it is possible to use the PUDC_B signal pin, which I am not going to use in my carrier card, as a signal pin. Although I have empty pins I want to complete the banks 34 and 35.

 

Thank you in advance

 

Víctor

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Victor,

    With your unused signals I would suggest you pull them out to a pad incase later down the line you need access to them. So long as you do not  set any of them as inputs you will not recieve any noise.

    As for the PUDC_B signal pin make sure you do not allow this pin to float before and during configuration. To determine if it is dual use please refer to Xilinx supporting document UG865.

    http://www.xilinx.com/support/documentation/user_guides/ug865-Zynq-7000-Pkg-Pinout.pdf 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Thanks Josh,

     

    About pulling the unused signals out to a pad was my first idea so I will do it. What is an interesting point is your comment about no to set those pins as inputs to avoid any noise.

     

    As for the PUDC_B signal pin, I am using it as an input, taking into account that the Microzed already has that signal pulled up, so in this way I consider I would not leave this pin (net) to float before and during configuration.

     

    Regards

     

    Víctor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Thanks Josh,

     

    About pulling the unused signals out to a pad was my first idea so I will do it. What is an interesting point is your comment about no to set those pins as inputs to avoid any noise.

     

    As for the PUDC_B signal pin, I am using it as an input, taking into account that the Microzed already has that signal pulled up, so in this way I consider I would not leave this pin (net) to float before and during configuration.

     

    Regards

     

    Víctor