Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design A clarification on Ethernet
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 709 views
  • Users 0 members are here
Related

A clarification on Ethernet

100jaime
100jaime over 9 years ago

Hi, new to the forum and to the microzed.

I have a question (obviously :) ), i hope this is the right subforum for it, apologies if it is not.

So, i am trying to develop a ethernet application, to begging with i started reading the hardware guide for the microzed and read that the phy is connected to the mac in the PS directly to the MIO pins. Thus, there s no need for PL for the connections, right?

So, in my case, im using vivado, does that mean that to set up the PL side of thinks you just need to create a block diagram, instantiate the zynq ip, run block automate, ensure eth0 is enable (it is by default), and the just genereta the bitstream and move onto the PS code development?

Im addig an image of my current setUp in vivado:  https://ibb.co/dOpECa

Fullscreen contentimage_84522.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Thanks for your help.

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 9 years ago +1 verified
    Hello Jaime, That is correct! You may also want to take a look at the example designs located here for the MicroZed. http://ethernetfmc.com/exampledesigns/ They are done with an FMC Carrier Card and FMC…
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Jaime,

    That is correct! You may also want to take a look at the example designs located here for the MicroZed. http://ethernetfmc.com/exampledesigns/

    They are done with an FMC Carrier Card and FMC Module, but you should be able to take the principles away for it.

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • 100jaime
    0 100jaime over 9 years ago

    Sorry for the late respond, I read it in the phone and forgot to unswer you.

    Thanks for the info and the link :)