Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Run .elf issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 1246 views
  • Users 0 members are here
Related

MicroZed Run .elf issue

e14 Contributor
e14 Contributor over 10 years ago

I am currently building a system to run on the MicroZed 7020 board. My system consists of an FPGA design and a baremetal application. I've used Vivado 2014.4 but a week ago I decided to try the new Vivado 2016.1. I didn't realize at that time that I need 2016.1 compatible board definition files. I went through the hazzle of updating everything in my design and got the bitstream generated. After some time spent with the SDK and multiple tries to run my app I remembered the board definition files and noticed that there isn't ones for 2016.1. So I decided to go back and continue with my 2014.4 version. Now when running my system with the 2014.4 version I got this weird problem. When programming the FPGA and running my application for the first time after a power-cycle everything goes smoothly. When I want to relaunch the app it seems that the FPGA is reset even though I haven't specified the run configurations to reset the whole system. The launch is interrupted with the message

No Target with ID 64 in the System

Unexpected error while launching program.
java.lang.RuntimeException: Failed to download ELF file

Cannot access JTAG-DP: invalid ACK value (0x00, expected=0x02)
Error Address = 0x0017b000, Size = 0x00000004

at com.xilinx.sdk.targetmanager.internal.TM.downloadELF(TM.java:666)
at com.xilinx.sdk.debug.core.internal.AppRunner.run(AppRunner.java:129)
at com.xilinx.sdk.debug.core.XilinxAppLaunchConfigurationDelegate.runApplication(XilinxAppLaunchConfigurationDelegate.java:605


If I reprogram the FPGA and relaunch the app SDK thinks I have another session in progress and I need to relaunch SDK.

If I modify the run configurations so that SDK resets the whole system and programs the FPGA on every relaunch I have to relaunch twice as the first relaunch is always interrupted with the message "Unexpected error while launching program: Failed to download the bit file"

This is so impractical that I uninstalled 2016.1 and reinstalled 2014.4 hoping that it would fix the issue. No luck. Any ideas what trace did the 2016.1 leave on my computer/board?

BR,
Esa


  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    *Did you use a base reference design?
    *Are you certain you removed all the modifications you made when trying to use 2016.1?
    *Can you first make a backup of your project folder, then try to delete all Vivado generated files.  Next rebuild your project in Vivado 2014.4?  It is quite possible that there are binaries or configuration files generated by Vivado that are incompatible going backwards to 2014.4 from 2016.1.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to drozwood90

    Thank you Dan for your response,

    My Vivado Block design uses the basic Zynq Processing System which is connected to AXI Lite IPs which I have generated from my VHDL sources. I think that the SDK application project may have been built on the Hello World -example rather than an Empty Project.

    When moving to 2016.1 I archived my 2014.4 designs and updated all the IPs after which I was able to generate the bitstream. When I left the 2016.1 alone I extracted the 2014.4 version and continued with that one. It didn't work and so I packaged all the IPs and built the system block design with the 2014.4 from scratch. I exported the new hardware and made a new SDK project but it didn't make any difference. So to my knowledge there should not be any 2016.1 files in my project.

    -Esa

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to drozwood90

    Thank you Dan for your response,

    My Vivado Block design uses the basic Zynq Processing System which is connected to AXI Lite IPs which I have generated from my VHDL sources. I think that the SDK application project may have been built on the Hello World -example rather than an Empty Project.

    When moving to 2016.1 I archived my 2014.4 designs and updated all the IPs after which I was able to generate the bitstream. When I left the 2016.1 alone I extracted the 2014.4 version and continued with that one. It didn't work and so I packaged all the IPs and built the system block design with the 2014.4 from scratch. I exported the new hardware and made a new SDK project but it didn't make any difference. So to my knowledge there should not be any 2016.1 files in my project.

    -Esa