Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Run .elf issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 1246 views
  • Users 0 members are here
Related

MicroZed Run .elf issue

e14 Contributor
e14 Contributor over 10 years ago

I am currently building a system to run on the MicroZed 7020 board. My system consists of an FPGA design and a baremetal application. I've used Vivado 2014.4 but a week ago I decided to try the new Vivado 2016.1. I didn't realize at that time that I need 2016.1 compatible board definition files. I went through the hazzle of updating everything in my design and got the bitstream generated. After some time spent with the SDK and multiple tries to run my app I remembered the board definition files and noticed that there isn't ones for 2016.1. So I decided to go back and continue with my 2014.4 version. Now when running my system with the 2014.4 version I got this weird problem. When programming the FPGA and running my application for the first time after a power-cycle everything goes smoothly. When I want to relaunch the app it seems that the FPGA is reset even though I haven't specified the run configurations to reset the whole system. The launch is interrupted with the message

No Target with ID 64 in the System

Unexpected error while launching program.
java.lang.RuntimeException: Failed to download ELF file

Cannot access JTAG-DP: invalid ACK value (0x00, expected=0x02)
Error Address = 0x0017b000, Size = 0x00000004

at com.xilinx.sdk.targetmanager.internal.TM.downloadELF(TM.java:666)
at com.xilinx.sdk.debug.core.internal.AppRunner.run(AppRunner.java:129)
at com.xilinx.sdk.debug.core.XilinxAppLaunchConfigurationDelegate.runApplication(XilinxAppLaunchConfigurationDelegate.java:605


If I reprogram the FPGA and relaunch the app SDK thinks I have another session in progress and I need to relaunch SDK.

If I modify the run configurations so that SDK resets the whole system and programs the FPGA on every relaunch I have to relaunch twice as the first relaunch is always interrupted with the message "Unexpected error while launching program: Failed to download the bit file"

This is so impractical that I uninstalled 2016.1 and reinstalled 2014.4 hoping that it would fix the issue. No luck. Any ideas what trace did the 2016.1 leave on my computer/board?

BR,
Esa


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Esa,

     

    I don't have any information on your designs or the IP you use but there can be issues as you move to newer versions of the Xilinx tools. If you are starting your design now I would suggest starting with the latest tool suite, 2016.1 in this case.

     

    As mentioned above I was able to verify that the 2015.4 board files work with 2016.1. It is possible that your 2016.1 Vivado/SDK installation download was corrupted. You should always check the MD5 sum of the downloaded file prior to performing the installation. I would suggest implementing one of the 'canned' SDK applications, such as the peripheral test, for your exported hardware design to verify your tool installation and hardware setup.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Esa,

     

    I don't have any information on your designs or the IP you use but there can be issues as you move to newer versions of the Xilinx tools. If you are starting your design now I would suggest starting with the latest tool suite, 2016.1 in this case.

     

    As mentioned above I was able to verify that the 2015.4 board files work with 2016.1. It is possible that your 2016.1 Vivado/SDK installation download was corrupted. You should always check the MD5 sum of the downloaded file prior to performing the installation. I would suggest implementing one of the 'canned' SDK applications, such as the peripheral test, for your exported hardware design to verify your tool installation and hardware setup.

     

    -Gary