Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Run .elf issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 1243 views
  • Users 0 members are here
Related

MicroZed Run .elf issue

e14 Contributor
e14 Contributor over 10 years ago

I am currently building a system to run on the MicroZed 7020 board. My system consists of an FPGA design and a baremetal application. I've used Vivado 2014.4 but a week ago I decided to try the new Vivado 2016.1. I didn't realize at that time that I need 2016.1 compatible board definition files. I went through the hazzle of updating everything in my design and got the bitstream generated. After some time spent with the SDK and multiple tries to run my app I remembered the board definition files and noticed that there isn't ones for 2016.1. So I decided to go back and continue with my 2014.4 version. Now when running my system with the 2014.4 version I got this weird problem. When programming the FPGA and running my application for the first time after a power-cycle everything goes smoothly. When I want to relaunch the app it seems that the FPGA is reset even though I haven't specified the run configurations to reset the whole system. The launch is interrupted with the message

No Target with ID 64 in the System

Unexpected error while launching program.
java.lang.RuntimeException: Failed to download ELF file

Cannot access JTAG-DP: invalid ACK value (0x00, expected=0x02)
Error Address = 0x0017b000, Size = 0x00000004

at com.xilinx.sdk.targetmanager.internal.TM.downloadELF(TM.java:666)
at com.xilinx.sdk.debug.core.internal.AppRunner.run(AppRunner.java:129)
at com.xilinx.sdk.debug.core.XilinxAppLaunchConfigurationDelegate.runApplication(XilinxAppLaunchConfigurationDelegate.java:605


If I reprogram the FPGA and relaunch the app SDK thinks I have another session in progress and I need to relaunch SDK.

If I modify the run configurations so that SDK resets the whole system and programs the FPGA on every relaunch I have to relaunch twice as the first relaunch is always interrupted with the message "Unexpected error while launching program: Failed to download the bit file"

This is so impractical that I uninstalled 2016.1 and reinstalled 2014.4 hoping that it would fix the issue. No luck. Any ideas what trace did the 2016.1 leave on my computer/board?

BR,
Esa


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Esa,

     

    I just tried a 2016.1 design for the MicroZed 7020 (just a basic design) and exported to 2016.1 SDK. I used the 2015.4 MicroZed 7020 board defintion files. You should be able to install them in the Vivado 2016.1 install OK. Just follow the 2015.4 instructions, using the 2016.1 installation directory.

     

    I build the canned 'peripherial test' application. I was able to load and run/debug the the application with no issues. I did click the 'disconnect' icon on the Debug tool bar before relaunching the application in the SDK debugger the second time. 

     

    Run ps7_init and Run ps7-post_config were checked in the Debug configuration.

     

    You might want to try one of the 'canned' SDK applications to verify that your board and Vivado/SDK installation are all good before trying your application.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Gary and thank you for your response,

    Actually I tried the 2015.4 board definition files on my 2016.1 installation and I could not get my system running. I'm not sure in which part of the processor reset the error appeared in 2016.1 as I was able to program the FPGA (blue led on) but I couldn't get the application to launch at any point. Not sure If should package all my designs in 2016.1 from scratch and try again as I'm a bit uncertain about the IP Update. Then again how could that have an effect on the SDK application...?

    -Esa

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Gary and thank you for your response,

    Actually I tried the 2015.4 board definition files on my 2016.1 installation and I could not get my system running. I'm not sure in which part of the processor reset the error appeared in 2016.1 as I was able to program the FPGA (blue led on) but I couldn't get the application to launch at any point. Not sure If should package all my designs in 2016.1 from scratch and try again as I'm a bit uncertain about the IP Update. Then again how could that have an effect on the SDK application...?

    -Esa