Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design No external XADC VREF/VCC  sourcing options?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 308 views
  • Users 0 members are here
Related

No external XADC VREF/VCC  sourcing options?

smvo555
smvo555 over 11 years ago

Hi guys,

So there is no option to use an external voltage reference for the XADC using the microzed? If there is not then what is the purpose of the regulators on the IO carrier card for the XADC VCC and VREF?

Thanks,

Sam

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Response from the IO Carrier designer:

     

    "The MicroZed SOM can be operated stand-alone without a carrier via USB.  The Zynq requires an ADC reference voltage.  For this reason, the ADC on MicroZed SOMs are set to 1.8V.  The 1.8V reference on the IOCC matches this value on CON1. "

     

    So the voltages on the IO Carrier Card are there to provide the required voltages on CON1 and are set to match the MicroZed values.

    -Gary