Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design USB dongles not enumerating
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 1217 views
  • Users 0 members are here
Related

USB dongles not enumerating

e14 Contributor
e14 Contributor over 10 years ago

Hi, I am having problems with a couple of WI-FI USB dongles that, when connected to the microzed board running Linux, do not get enumerated (the protocol is stuck very very early in the process).
If I put an hub in between all works fine.
Has anyone experienced anything like this? many other dongles work flawlessly but two of them (D-Link DWA-140 and Edimax EW-7718uN) don't.
Obiously the two dongles work everywhere else.

The same problem replicates on our custom board that was developed as a close copy of the microzed so it must be a design or component problem (phy related?)

Any information would be very much appreciated,
thanks
Jo

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hey Gary.

    I don't think that it could be a power problem, because when the (unpowered) hub is in between, it can easily handle not one, but three dongles, including the mentioned two that without the hub would not work.


    Jo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hey Gary.

    I don't think that it could be a power problem, because when the (unpowered) hub is in between, it can easily handle not one, but three dongles, including the mentioned two that without the hub would not work.


    Jo