Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design USB dongles not enumerating
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 1217 views
  • Users 0 members are here
Related

USB dongles not enumerating

e14 Contributor
e14 Contributor over 10 years ago

Hi, I am having problems with a couple of WI-FI USB dongles that, when connected to the microzed board running Linux, do not get enumerated (the protocol is stuck very very early in the process).
If I put an hub in between all works fine.
Has anyone experienced anything like this? many other dongles work flawlessly but two of them (D-Link DWA-140 and Edimax EW-7718uN) don't.
Obiously the two dongles work everywhere else.

The same problem replicates on our custom board that was developed as a close copy of the microzed so it must be a design or component problem (phy related?)

Any information would be very much appreciated,
thanks
Jo

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The Linux I'm using comes with Yocto Dora and the kernel version is 3.8.11.
    The Xilinx layer comes from github.com/architech-boards/meta-xilinx.git (so it's not Petalinux).

    The problem appears very consistently on the zedboard, microzed and our custom boards even if they are equipped with different PHYs.

    j

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The Linux I'm using comes with Yocto Dora and the kernel version is 3.8.11.
    The Xilinx layer comes from github.com/architech-boards/meta-xilinx.git (so it's not Petalinux).

    The problem appears very consistently on the zedboard, microzed and our custom boards even if they are equipped with different PHYs.

    j