Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design confused about axi ps-pl interfacing
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 2753 views
  • Users 0 members are here
Related

confused about axi ps-pl interfacing

smvo555
smvo555 over 12 years ago

Hi everyone, (any one please!)

I'm not great with processor architectures and software development.

I've been trying to get a simple application running where an HDL module controls the state of the user LED.
I can do this on the processor side, but I haven't been able to have the processor check the state of my HDL port.

I know there are a number of ways to do this, like sharing dual port RAM, I would like to implement the most direct method, which I think is using the EMIO directly.

Please correct my understanding of this:  

When I enable the EMIO in the Zynq7 Processing System a port is created called GPIO_0. I specified the width as 1, and connected it to my HDL modules port in the wrapper.
So in the application, I should be able to check the state of MIO 54, the first EMIO pin. However when I do this the value is 0, which isn't correct.

Okay, so do I need to connect the AXI interconnect for this? How would this be done to have the PS check the state of a PL port? Do I need to instantiate the AXI in the wrapper as well as in the block design?

Any guidance is much appreciated, I've been at this for a while now trying to get my head around the AXI

Thanks

Sam

  • Sign in to reply
  • Cancel
Parents
  • smvo555
    0 smvo555 over 12 years ago

    I think I need to add a AXI GPIO interface in the HDL code so I can connect it to the master of the AXI interconnect, however I'm confused about how the EMIO plays into this because the EMIO is not a master or a slave on the ZYNQ7 Processing System block and thus I can't connect it to an AXI slave port.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • smvo555
    0 smvo555 over 12 years ago

    I think I need to add a AXI GPIO interface in the HDL code so I can connect it to the master of the AXI interconnect, however I'm confused about how the EMIO plays into this because the EMIO is not a master or a slave on the ZYNQ7 Processing System block and thus I can't connect it to an AXI slave port.