Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design No AXI bus on Vivado 2013.3 for MIcrozed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 431 views
  • Users 0 members are here
Related

No AXI bus on Vivado 2013.3 for MIcrozed board

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I have some problem with Vivado 2013.3 and Microzed. when I add any AXI IP (for example a simple AXI_GPIO) I can only see the "run connection automation" for the IO, but there is no "run block automation" that automatically create an AXI bus to connect the AXI IP to the processing system.

In turn, if select the Zedboard instead of Microzed, everything works fine!

how is that possible!?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I've just found out that when I run the connection automation for the processing system, the master axi disappears from the processing system!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    They might have just forgot to add it to their preset file for the microzed, but the axi bus can not magically not be there. So just customize your processing system and within the PS-PL config. add the GP Master AXI Interface (Select -> M AXI GP0 interface).