Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed randomly resetting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 364 subscribers
  • Views 1099 views
  • Users 0 members are here
Related

MicroZed randomly resetting

e14 Contributor
e14 Contributor over 12 years ago

Microzed randomly resets.  Rarely running more than 24 hours.  Sometimes resetting every few minutes. 

Reset frequency possibly a function of activity.  MicroZed powered from USB.  Maybe some power valid sensor is triggering a reset??

Anybody else seen this?

llj

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Could it be that your design exceeds the power available through the USB port? 

     

    By USB specification a single USB port can only supply a maximum of 500 mA @ 5V. By the time you power the PS section of the Zynq device, the DDR memory and the other components on the MicroZed board there is a limited amount of current left to power the PL section of the Zynq, any loads on the USB-Host interface, and anything plugged into the PMOD connector.

     

    If this is a possible source of your resets there are several ways to provide additional power to the MicroZed.

     

    Use a USB Y-cable, with two connections to the Host for a 1A source.

    Populating a DC barrel jack (J4) and providing 5V there.

    Plug the MicroZed into a carrier card to provide additional power.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Could it be that your design exceeds the power available through the USB port? 

     

    By USB specification a single USB port can only supply a maximum of 500 mA @ 5V. By the time you power the PS section of the Zynq device, the DDR memory and the other components on the MicroZed board there is a limited amount of current left to power the PL section of the Zynq, any loads on the USB-Host interface, and anything plugged into the PMOD connector.

     

    If this is a possible source of your resets there are several ways to provide additional power to the MicroZed.

     

    Use a USB Y-cable, with two connections to the Host for a 1A source.

    Populating a DC barrel jack (J4) and providing 5V there.

    Plug the MicroZed into a carrier card to provide additional power.

     

    -Gary