Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Heat Management
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 362 subscribers
  • Views 1417 views
  • Users 0 members are here
Related

Heat Management

e14 Contributor
e14 Contributor over 12 years ago

I believe that in theory the Zynq chip on a AES-Z7MB-7Z010-G can become excessively hot if the PL and PS is operating at full capacity.

If that happens, what are the recommended heatsinks and/or fans.

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have the 7Z020 MicroZed and the Zynq definitely is getting quite hot before I've put any of my own logic in the PL.  I'm definitely skeptical of the wisdom of using a 19mm square heat sink due to the proximity of the capacitors which are taller than the BGA.  I'm going to try the Wakefield Thermal Solutions LTN20069-T5, which is 16.5mm square by 8.9mm, supplied with thermal adhesive tape.  While the Cool Innovations is better, the Wakefield is available from stock and is quite inexpensive (under $1.50 in quantity 1).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have the 7Z020 MicroZed and the Zynq definitely is getting quite hot before I've put any of my own logic in the PL.  I'm definitely skeptical of the wisdom of using a 19mm square heat sink due to the proximity of the capacitors which are taller than the BGA.  I'm going to try the Wakefield Thermal Solutions LTN20069-T5, which is 16.5mm square by 8.9mm, supplied with thermal adhesive tape.  While the Cool Innovations is better, the Wakefield is available from stock and is quite inexpensive (under $1.50 in quantity 1).