Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Unable to program Microzed through Carrier Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 687 views
  • Users 0 members are here
Related

Unable to program Microzed through Carrier Card

e14 Contributor
e14 Contributor over 10 years ago

I have the Microzed SOM cost optimized board which can be powered up only through a Carrier card. I have the Microzed Carrier card kit for Arduino to which I have plugged my Microzed Board. When I connect the JTAG cable to the Carrier card using my Laptop, 2 LEDS glow indicating that the Carrier card is powered on through the Microzed board. But When I try to program the Microzed board, I get the following error:

ERROR: [Labtoolstcl 44-26] No hardware targets exist on the server [localhost]
Check to make sure the cable targets connected to this machine are properly connected and powered up, then use the disconnect_hw_server and connect_hw_server commands
to re-register the hardware targets

Since there are no LEDS mounted on the MicroZed board, I do not know if the board is getting powered up or not. I'm using  Windows 7 64 bit OS. I'm using Vivado 2015.4 version. The JTAG cable is the one provided along with the carrier card. 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

     

    The Cost Optimized MicroZed also requires a JTAG connection from the Carrier Card. While the MicroZed FMC Carrier Card and the MicroZed IO Carrier Card do provide a JTAG connector, the MicroZed Arduino Carrier Card and MicroZed Breakout Carrier Card do not. The only way to connect to a cost optimized MicroZed on an Arduino Carrier Card to JTAG would be to install a connector at the J3 location of the cost optimized MicroZed. The boot options are also fixed to QSPI boot on the cost optimized MicroZed as well. The cost optimized MicroZed was meant for a specific production use case and not for development or debug. You probably want to just use a standard MicroZed board with a J3 JTAG connector.

     

    You will also need a JTAG programming cable as none of the MicroZed board have integrated JTAG programming logic. I would suggest an HS3 programming cable:

     

    http://products.avnet.com/shop/en/ema/development-tools/3074457345625071215

    https://store.digilentinc.com/jtag-hs3-programming-cable/

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank you for your reply Gary. When you say that the cost optimized board requires a Jtag connection from carrier card, do you mean that I need to install a connector on J3 of the microzed board, and connect the port to my laptop using the cable you have suggested?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank you for your reply Gary. When you say that the cost optimized board requires a Jtag connection from carrier card, do you mean that I need to install a connector on J3 of the microzed board, and connect the port to my laptop using the cable you have suggested?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Yes, if your carrier card does not have a JTAG connector you will need to install the one on the MicroZed. You may also want to remove the default connections and install Jumper Pins for JP1, JP2, and JP3 on the MicroZed board so that you can use jumpers to select the boot mode. On the cost optimized MicroZed the boot mode is fixed to QSPI mode.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank you for all the clarifications Gary. We have decided to order a Microzed kit and work with that.