Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed z7020 with Petalinux 2021.2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 360 subscribers
  • Views 2081 views
  • Users 0 members are here
  • Report Bug
Related

Microzed z7020 with Petalinux 2021.2

100jnikolai
100jnikolai over 4 years ago

Hi there,

I've been trying to get a Microzed z7020 board to work with the latest version of Petalinux 2021.2.  Currently I am using 2018.2 without issue.  I am able to perform the following to create a new setup without issue, just as before:

petalinux-create -t project --template zynq --name mz7020_qspi

petalinux-config --get-hw-description [path to .xsa file here]

However, when I try to build with:

petalinux-package --boot --u-boot --kernel --fpga

I always get the following output:

[INFO] Sourcing buildtools

INFO: Getting system flash information...

INFO: File in BOOT BIN: "/home/james/Download/petalinux/mz7020_qspi/images/linux/zynq_fsbl.elf"

INFO: File in BOOT BIN: "/home/james/Download/petalinux/mz7020_qspi/project-spec-hw-description/design_1_wrapper.bit"

INFO: File in BOOT BIN: "/home/james/Download/petalinux/mz7020_qspi/images/linux/u-boot.elf"

INFO: File in BOOT BIN: "/home/james/Download/petalinux/mz7020_qspi/images/linux/system.dtb"

INFO: File in BOOT BIN: "/home/james/Download/petalinux/mz7020_qspi/images/linux/boot.scr"

INFO: File in BOOT BIN: "/home/james/Download/petalinux/mz7020_qspi/images/linux/image.ub"

INFO: Generating zynq binary package BOOT.BIN...

****** Xilinx Bootgen v2021.2

  **** Build date : Sep 30 2021-06:08:18

     ** Copyright 1986-2021 Xilinx, Inc. All Rights Reserved.

[ERROR]   : Section image.ub.0.offset of 0x520000 overlaps with prior section end address of FC0AC0

ERROR: Fail to create BOOT image

I've seen elsewhere that this could be related to the size of the boot partition, so if I run petalinux-config, then go to:

Subsystem AUTO Hardware Settings -> Flash Settings

I change:

(boot) name

(0x500000) size

   *** partition 1 ***

(bootenv) name

(0x20000) size

   *** partition 2 ***

(kernel) name

(0xA80000) size

   *** partition 3 ***

(spare) name

(0x0) size

   *** partition 4 ***

() name

on the following lines to:

(boot) name

(0x1000000) size

to increase the size of said partition.  Then I run a petalinux-build and try again with petalinux-package without issue.

At that point, the issue seems to be that the BOOT.bin is too large to flash onto the onboard memory of the Microzed.  When I attempt to flash the image within the Vitis environment (formerly Xilinx SDK), I get the following:

Performing Erase Operation...
sf erase 0 1CA0000


ERROR: attempting erase past flash size (0x1000000)

Zynq> f erase 0 1CA0000


Erase Operation failed.
INFO: [Xicom 50-44] Elapsed time = 0 sec.

ERROR: Flash Operation Failed

I use flash type qspi_single, as it seems to be the only type that is fully compatible.  If I try qspi_dual_parallel, qspi_dual_stacked, or nor, it seems to flash without issue, but then once I try to bootup the Microzed it either doesn't at all or comes back with:

*** Warning - bad CRC, using default environment

In: serial@e0001000
Out: serial@e0001000
Err: serial@e0001000
Net:
ZYNQ GEM: e000b000, mdio bus e000b000, phyaddr -1, interface rgmii-id
eth0: ethernet@e000b000
Hit any key to stop autoboot: 0
SF: Detected s25fl128s with page size 256 Bytes, erase size 64 KiB, total 16 MiB
device 0 offset 0xfc0000, size 0x40000
SF: 262144 bytes @ 0xfc0000 Read: OK
QSPI: Trying to boot script at 3000000
## Executing script at 03000000
Trying to load boot images from qspi
SF: Detected s25fl128s with page size 256 Bytes, erase size 64 KiB, total 16 MiB
Offset exceeds device limit
sf - SPI flash sub-system

...

...

I thought that there was 64mb of flash at least, but this seems to act more like 16mb.  I could definitely be wrong about the storage size.  Am I possibly misconfiguring anything obvious and/or flashing it the wrong way?  Before the change to distro-boot with 2020.1 apparently, it would work flawlessly with 2018.2.  Any help would be greatly appreciated and I can lookup anything that would be helpful.