Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed PetaLinux 2023.2 spidev transfer timed out
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 361 subscribers
  • Views 526 views
  • Users 0 members are here
Related

MicroZed PetaLinux 2023.2 spidev transfer timed out

acountryman25
acountryman25 over 1 year ago

This question has also been posted to the AMD Adaptive Support forums (https://adaptivesupport.amd.com/s/question/0D5KZ00000pAdsk0AC/zynq-7000-petalinux-20232-spidev-transfer-timed-out).

The team I am a member of is currently working on upgrading a project we inherited from the 2014 tools (Vivado, PetaLinux, etc) to the 2023.2 tools. This project uses PetaLinux running on an Avnet MicroZed AES-Z7MB-7Z020-SOM-G (XC7Z020-1CLG400C). We have encountered an issue with SPI 1 that we have not been able to resolve ("spidev spi1.X: SPI transfer timed out", "spi_master spi1: failed to transfer one message from queue", the state of the SPI 1 pins/signals has been checked and they are in their idle state with no activity observed).

The PetaLinux 2023.2 project was created using the scripts/make_mz7020_som_base.sh script from the Avnet petalinux GitHub repository's 2023.2 branch. The following changes have been made to the petalinux and meta-avnet repositories:

  • Made various modifications so that the build can be performed without internet access.
  • Made the following build configuration changes:
    • Changed BOOT_METHOD to INITRD
    • Set BOOT_SUFFIX to _MINIMAL
    • Set INITRAMFS_IMAGE to petalinux-image-minimal
  • Removed axi_intc_0 and amba_pl entries from meta-avnet/recipes-bsp/device-tree/files/mz/system-bsp.dtsi to fix rebuild errors that occur when the XSA file is swapped out for the one from our Vivado project.

SPI transfers are done using SPI_IOC_MESSAGE ioctl() calls.

SPI 1 is configured as follows in Vivado:

  • SPI 1 is enabled and is configured to use MIO 10 .. 15
    • MIO 10:
      • Signal: mosi
      • IO Type: LVCMOS 3.3V
      • Speed: slow
      • Pullup: disabled
      • Direction: inout
    • MIO 11:
      • Signal: miso
      • IO Type: LVCMOS 3.3V
      • Speed: slow
      • Pullup: enabled
      • Direction: inout
    • MIO 12:
      • Signal: sclk
      • IO Type: LVCMOS 3.3V
      • Speed: slow
      • Pullup: disabled
      • Direction: inout
    • MIO 13:
      • Signal: ss[0]
      • IO Type: LVCMOS 3.3V
      • Speed: slow
      • Pullup: enabled
      • Direction: inout
    • MIO 14:
      • Signal: ss[1]
      • IO Type: LVCMOS 3.3V
      • Speed: slow
      • Pullup: enabled
      • Direction: out
    • MIO 15:
      • Signal: ss[2]
      • IO Type: LVCMOS 3.3V
      • Speed: slow
      • Pullup: enabled
      • Direction: out

dtsi SPI 1 configuration overrides:

&spi1 {
    status = "okay";
    num-cs = <3>;
    is-decoded-cs = <0>;
    speed-hz=<10000000>;
 
    device@0{
        status = "okay";
        compatible="rohm,dh2228fv";   // Not actually this device, workaround to get /dev/spidev1.0 to appear.
        reg=<0>;                      // Chipselect 0
        spi-max-frequency=<10000000>; // 10 Mhz
    };
 
    device@1{
        status = "okay";
        compatible="rohm,dh2228fv";   // Not actually this device, workaround to get /dev/spidev1.0 to appear.
        reg=<1>;                      // Chipselect 1
        spi-max-frequency=<10000000>; // 10 Mhz
    };
 
    device@2{
        status = "okay";
        compatible="rohm,dh2228fv";   // Not actually this device, workaround to get /dev/spidev1.0 to appear.
        reg=<2>;                      // Chipselect 2
        spi-max-frequency=<10000000>; // 10 Mhz
    };
};

SPI 1 device tree entry from decompiled DTB:

spi@e0007000 {
    compatible = "xlnx,zynq-spi-r1p6";
    reg = <0xe0007000 0x1000>;
    status = "okay";
    interrupt-parent = <0x04>;
    interrupts = <0x00 0x31 0x04>;
    clocks = <0x01 0x1a 0x01 0x23>;
    clock-names = "ref_clk\0pclk";
    #address-cells = <0x01>;
    #size-cells = <0x00>;
    num-cs = <0x03>;
    is-decoded-cs = <0x00>;
    speed-hz = <0x989680>;
    phandle = <0x24>;
 
    device@0 {
        status = "okay";
        compatible = "rohm,dh2228fv";
        reg = <0x00>;
        spi-max-frequency = <0x989680>;
    };
 
    device@1 {
        status = "okay";
        compatible = "rohm,dh2228fv";
        reg = <0x01>;
        spi-max-frequency = <0x989680>;
    };
 
    device@2 {
        status = "okay";
        compatible = "rohm,dh2228fv";
        reg = <0x02>;
        spi-max-frequency = <0x989680>;
    };
};

We have tried the following to resolve this issue but they were not successful:

  • Disabling power management in the kernel configuration as suggested by some adaptivesupport posts
  • Increasing the timeout period as was done for https://adaptivesupport.amd.com/s/article/2021-Zynq-7000-Zynq-MPSoC-Versal-Yocto-PetaLinux-kernel-driver-fails-to-configure?language=en_US
  • Changing the SPI 1 interrupts configuration (<0 49 4>) to the configuration that was used in the old device tree (<0 49 0>)

Any suggestions for resolving this issue would be greatly appreciated.