Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Wilink8 on Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 360 subscribers
  • Views 268 views
  • Users 0 members are here
Related

Wilink8 on Microzed

mariooook
mariooook over 7 years ago

Hello,

 

I want to setup the Wilink8 Module on my Microzed following http://zedboard.org/sites/default/files/documentations/GSG-AES-PMOD-WILINK8-G-v1_6-1.pdf guide.

As far as I understand I have to execute "./microzed-wilink8-ramdisk.sh" This takes quiet long, however it always fails at u-boot stage.

 

cd /home/architech/Documents/u-boot-xlnx && arm-poky-linux-gnueabi-ld.bfd -L ~/architech_sdk/architech/microzed/toolchain/sysroots/armv7a-vfp-neon-poky-linux-gnueabi/usr/lib/arm-poky-linux-gnueabi/4.8.1/  -pie -T u-boot.lds --gc-sections -Bstatic -Ttext 0x4000000 arch/arm/cpu/armv7/start.o --start-group arch/arm/cpu/armv7/built-in.o arch/arm/cpu/armv7/zynq/built-in.o arch/arm/cpu/built-in.o arch/arm/lib/built-in.o board/xilinx/zynq/built-in.o common/built-in.o disk/built-in.o drivers/built-in.o drivers/dma/built-in.o drivers/gpio/built-in.o drivers/i2c/built-in.o drivers/input/built-in.o drivers/mmc/built-in.o drivers/mtd/built-in.o drivers/mtd/onenand/built-in.o drivers/mtd/spi/built-in.o drivers/net/built-in.o drivers/net/phy/built-in.o drivers/pci/built-in.o drivers/power/battery/built-in.o drivers/power/built-in.o drivers/power/fuel_gauge/built-in.o drivers/power/mfd/built-in.o drivers/power/pmic/built-in.o drivers/serial/built-in.o drivers/spi/built-in.o drivers/usb/eth/built-in.o drivers/usb/gadget/built-in.o drivers/usb/host/built-in.o drivers/usb/musb-new/built-in.o drivers/usb/musb/built-in.o drivers/usb/phy/built-in.o drivers/usb/ulpi/built-in.o fs/built-in.o lib/built-in.o lib/libfdt/built-in.o net/built-in.o test/built-in.o --end-group /home/architech/Documents/u-boot-xlnx/arch/arm/lib/eabi_compat.o  -L . -lgcc -Map u-boot.map -o u-boot

arm-poky-linux-gnueabi-ld.bfd: cannot find -lgcc

make: *** [u-boot] Error 1

 

The actual script causing this issue.

echo -e "\e[7;32m---------------------- U-Boot begin --------------------------------\e[0m"

 

cd ~/Documents

echo -e "\e[0;32m---- Get sources from Xilinx ---------------------------------------\e[0m"

git clone https://github.com/Xilinx/u-boot-xlnx.git

        ### change into the U-Boot source folder and checkout commit

cd u-boot-xlnx

 

echo -e "\e[0;32m---- Checkout a tested commit --------------------------------------\e[0m"

git checkout xilinx-v2014.2

### set cross-toolchain

source ~/architech_sdk/architech/microzed/toolchain/environment-nofs

export LDFLAGS="-L ~/architech_sdk/architech/microzed/toolchain/sysroots/armv7a-vfp-neon-poky-linux-gnueabi/usr/lib/arm-poky-linux-gnueabi/4.8.1/"

echo -e "\e[0;32m---- Build ---------------------------------------------------------\e[0m"

### clear any stale build configurations

make ARCH=arm distclean

 

### set the Zed build configuration

make zynq_microzed_config

 

### Build U-Boot

make all

 

echo -e "\e[7;32m---------------------- U-Boot end ----------------------------------\e[0m"

echo -e "\e[7;32m---- File generated: -----------------------------------------------\e[0m"

echo -e "\e[7;32m---- ~/Documents/u-boot-xlnx/u-boot --------------------------------\e[0m"

 

 

 

 

Does anyone know what to do? I got the newest gcc-multilib and I am using the Architech virtual box image. I guess that is supposed to work out of the box anyway?

 

BR