Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PCIe AHCI Mass Storage
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 354 subscribers
  • Views 631 views
  • Users 0 members are here
Related

PCIe AHCI Mass Storage

e14 Contributor
e14 Contributor over 12 years ago

Hi

anyone had any luck with any PCIe AHCI card?

we are using Plextor SSD, and it seems to have problems on desktop PCs, we see the same.

Is the problem related to Plextor, or is the problem some generic issue with Xilinx PCIe?

http://www.plextoramericas.com/index.php/forum/27-ssd/9007-plextor-m6e-not-working-in-linux-or-freebsd

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    no, no issues- the AHCI M2 SSD can be used with Xilinx PCIe root, no quirks patches or custom drivers needed. It just works.

    ata1: SATA link up 6.0 Gbps (SStatus 133 SControl 300)
    ata1.00: ATA-8: PLEXTOR PX-G128M6e, 1.03, max UDMA/133
    ata1.00: 250069680 sectors, multi 1: LBA48 NCQ (depth 31/32), AA
    ata1.00: configured for UDMA/133
    scsi 0:0:0:0: Direct-Access     ATA      PLEXTOR PX-G128M 1.03 PQ: 0 ANSI: 5
    sd 0:0:0:0: [sda] 250069680 512-byte logical blocks: (128 GB/119 GiB)
    sd 0:0:0:0: [sda] Write Protect is off
    sd 0:0:0:0: [sda] Mode Sense: 00 3a 00 00
    sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
    sda: unknown partition table
    sd 0:0:0:0: Attached scsi generic sg0 type 0
    sd 0:0:0:0: [sda] Attached SCSI disk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Can you report on the SSD read/write performance via PCIe?

    Thanks.