Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Can not generate a proper u-boot for mini-itx
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 356 subscribers
  • Views 1292 views
  • Users 0 members are here
Related

Can not generate a proper u-boot for mini-itx

e14 Contributor
e14 Contributor over 9 years ago

Hi All,

I followed the tutorial (Ubuntu_on_Zynq_Mini-ITX_Tutorial_04) to install Ubuntu on my mini-itx 7100.

However, when I tried to generated u-boot, I got a serial of problems described above. 

1. Follow the extra instructions and get warnings:

arch/../configs/zynq_mitx_defconfig:2:warning: unexpected data
arch/../configs/zynq_mitx_defconfig:3:warning: unexpected data
arch/../configs/zynq_mitx_defconfig:4:warning: unexpected data

the zynq_mitx_defconfig:

CONFIG_SPL=y
+S:CONFIG_ARM=y
+S:CONFIG_ZYNQ=y
+S:CONFIG_TARGET_ZYNQ_MITX=y
CONFIG_OF_CONTROL=n
CONFIG_DEFAULT_DEVICE_TREE="zynq-mini-itx"

the u-boot-xlnx is download from GitHub and the branch is xilinx-v2014.4

I think that the defconfig file may be incorrect so I checked zynq_zed_defconfig find that they are quite different. Therefore,

2. I copy all contents of  zynq_zed_defconfig into zynq_mitx_defconfig and rm "+S:" of the original lines. I can generate u-boot this time but can not boot my mini-itx 7100 (program done led keeps flashing).

I also tried to follow other verisons of tutorials but get nothing. The  zynq_mitx_defconfig of tutorial 2013.3, tutorial 2014.4, tutorial 2015.3 are all different.

Any help is appreciated

  • Sign in to reply
  • Cancel
  • elliemellie
    0 elliemellie over 9 years ago

    Not sure if it will help, but I will try anyway. Last time I was installing Ubuntu on Zyng mini itx I followed Ubuntu_on_Zynq_Tutorial_03. There were a few issues here and there but I withstood them with some googling,

     

    Cheers
    Ellie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to elliemellie

    Hi Ellie,

    I tried the verision you suggest and get the following issue:

    make -C arch/arm/cpu/armv7/zynq/ u-boot.lds
    make[1]: Entering directory `/root/2013/u-boot-xlnx-xilinx-v2013.4/arch/arm/cpu/armv7/zynq'
    make[1]: *** No rule to make target `u-boot.lds'.  Stop.
    make[1]: Leaving directory `/root/2013/u-boot-xlnx-xilinx-v2013.4/arch/arm/cpu/armv7/zynq'
    make: *** [arch/arm/cpu/armv7/zynq/u-boot.lds] Error 2
     

    It seems the u-boot.lds file is not generated. Did you have that issue?

    Thank you very much for you reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 9 years ago

    Hi fuwenl,

    Have you tried building for the ZedBoard using "make zynq_zed_config"?

    That one should definitely work, so if it does not, then there is likely an issue with the build environment.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to zedhed

    Hi Kevin,

    Thank you for you reply.
    The zynq_zed_defconfig works perfectly. The two defconfig files are quite different. The zynq_mitx_defconfig is shown in my first post.

    Best wishes.