Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Re-customize IP preset not showing up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 355 subscribers
  • Views 2556 views
  • Users 0 members are here
Related

Re-customize IP preset not showing up

brc6
brc6 over 8 years ago

Hello,

 

We have acquired a Mini-ITX 7z100 board and are trying to set it up. We managed to install the board definition files for Vivado and create a new project for that board. However, after adding the Zynq7 PS to the block design, when we open the "Re-customize IP" dialog, there is no preset in the list for our board. The only presets that show up are for ZC702, ZC706 and ZedBoard (which are installed by default with Vivado). The "preset.xml" file is present in "C:\Xilinx\Vivado\2017.4\data\boards\board_files\mini_itx_7z100\1.0", but it seems to be ignored by Vivado.

 

Is it expected? If so, how are we suppose to customize the IP to match the board then?

 

There is a similar topic from 2014 posted in the PicoZed board, but with no solution to this specific problem:

http://zedboard.org/content/board-definition-and-recustomize-ip#comment-11096

 

BR

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello BR,

    You installed the "Zynq Mini-ITX Board Definition Files Vivado 2015.3 or later" correct?

    Did you follow the instruction tutorial located in that download to ensure everything was installed correctly?

    It appears you installed it in the correct path.

    Did you specify you wanted to use the board definition file during the creation of your project?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • brc6
    0 brc6 over 8 years ago in reply to jafoste4

    Josh,

     

    Yes, we've installed the version you quoted and it was correctly installed as the board appears in the new project wizard. We have even created a new project for that board, so the files are installed correctly.

     

    Our problem was that no board specific preset is showing up in the "Re-customize IP" dialog for the Zynq. After reading the board definition file document more thoroughly, it appears this is not a problem as the "Run Block Automation" command will actually find and apply the correct preset (even though it does not show up in the list!?). We've used other boards in the past, and there was always a preset for those boards in the "Re-customize IP" dialog after installing the correct files, so we were a bit confused this is not the case with this new board.

     

    So, problem is solved now. Thank you.

     

    BR