Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Failed to build petalinux system image with own sdk project
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 354 subscribers
  • Views 561 views
  • Users 0 members are here
Related

Failed to build petalinux system image with own sdk project

e14 Contributor
e14 Contributor over 11 years ago

Hi

I tried to build petalinux system image based on Your Zynq_Mini-ITX_PetaLinux_2014_4 tutorial. Firstly i created petalinux project, then configured it using my harwdare description from sdk.

When trying to build system (petalinux-build) i've received followed errors:

/PetaLinux/zynq_7z045/build/linux/u-boot/src/u-boot-plnx/include/flash.h:20:14: error: 'CONFIG_SYS_MAX_FLASH_SECT' undeclared here (not in a function)

/PetaLinux/zynq_7z045/build/linux/u-boot/src/u-boot-plnx/include/flash.h:20:14: error: 'CONFIG_SYS_MAX_FLASH_SECT' undeclared here (not in a function)

/PetaLinux/zynq_7z045/build/linux/u-boot/src/u-boot-plnx/include/environment.h:153:19: error: 'CONFIG_ENV_SIZE' undeclared here (not in a function)

/PetaLinux/zynq_7z045/build/linux/u-boot/src/u-boot-plnx/include/environment.h:153:19: error: 'CONFIG_ENV_SIZE' undeclared here (not in a function)

I don't know where to look for a solution, so I'll be very apriciate for any help.

Best regards
Marcin

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Marcin,

      I'm guessing that the hw you have imported into the PetaLinux project is missing components that are required by the software configuration you are trying to build.   Have you tried going through the tutorial using the embedded hw design?  This will help verify that each of the steps are understood, and if you do run into any problems it is much easier to determine the solution since we are working from the same, known good platform.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Marcin,

      I'm guessing that the hw you have imported into the PetaLinux project is missing components that are required by the software configuration you are trying to build.   Have you tried going through the tutorial using the embedded hw design?  This will help verify that each of the steps are understood, and if you do run into any problems it is much easier to determine the solution since we are working from the same, known good platform.

    Ron