Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design AXI Ethernet Subsystem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 354 subscribers
  • Views 1474 views
  • Users 0 members are here
Related

AXI Ethernet Subsystem

e14 Contributor
e14 Contributor over 11 years ago

Hi all,




I have been trying to use the AXI Ethernet Subsystem in the Mini ITX board but I fail to take the internal PHY out of reset.




The Ethernet Subsystem is connected to a FIFO which is responsible for the block reset. I'm running the the FIFO Interrupt Example that comes with the IP driver. The code gets stuck when checking for the MgtRdy bit. This seems to be because the on-chip PHY is not out of reset, since the PhyRstCmplt bit is also low.




The MGT_CLK interface is connected to the board VCO which is set up to generate a 125 MHz differential clock. The block is also connected to the board SFP.




In previous designs when I did not have a PHY (loopback setup using the MII/GMII interface) the core would work fine. This problem only came up when I instantiate the on-chip PHY. I tried using Vivado 2014.2 (1000BASE-X PCS/PMA) and Vivado 2015.1 (1G/2.5G Ethernet PCS/PMA) and no success in both cases.




Have anyone had a similar issue?
Is there any way to check if the VCO output is correct?




Thank you,
Gustavo


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    1) You may want to take a look at XAPP1082 (http://www.xilinx.com/support/documentation/application_notes/xapp1082-zynq-eth.pdf). It implements what you are trying to do. The design uses ETH DMA instead of FIFO, but it will give you a good idea on how this interface can be implemented in Zynq PL.

    2) To see if the on-board clock synthesizer is generating the 125MHz clock, you need a scope to look at it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    1) You may want to take a look at XAPP1082 (http://www.xilinx.com/support/documentation/application_notes/xapp1082-zynq-eth.pdf). It implements what you are trying to do. The design uses ETH DMA instead of FIFO, but it will give you a good idea on how this interface can be implemented in Zynq PL.

    2) To see if the on-board clock synthesizer is generating the 125MHz clock, you need a scope to look at it.