Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PS freezes when making use of PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 356 subscribers
  • Views 3385 views
  • Users 0 members are here
Related

PS freezes when making use of PL

cone83
cone83 over 10 years ago

I am encountering very odd problems with my new Mini-ITX board. Whenever I make use of a significant portion of the PL resources, the PS just freezes.

I have done quite a lot of debugging on this, and the only thing that seems to affect this problem is the amount of resources used. I have a test design that does a lot of useless computations. If I allow Vivado to optimize away all the useless stuff and hence greatly reduce the resource usage, then the CPU does not freeze. If I prevent the optimization and use 56% LUTs, then the CPU freezes immediately.

There are no timing timing violations or other errors reported by Vivado. I have now come to a point where I suspect that my Zynq might actually be damaged.

I have created a set of boot files for reproducing this error on a Mini-ITX with Zynq 7100. The boot files can be downloaded here:
https://mega.nz/#F!9hF0kQrZ!RfGgoTnCO0QOtp6MSUFZxg

When booting this configuration, U-boot only manages to print a few lines on UART before the CPU stalls. Usually the output looks like this:

--------------
U-Boot 2015.07-dirty (Apr 09 2016 - 11:32:21 +0200)

Model: Zynq Mini-ITX Board
DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size
--------------

Sometimes it even freezes before being able to print the first line. I would be really thankful if somebody could try out those boot files and report if this error also occurs on other Mini-ITX boards with Zynq 7100 SoCs.

Many thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    While I don't have a 7z100 version of the Mini-ITX here to work with I was able to get someone to try your project on their board. It got further than you post indicates but did hang at the 'Starting Kernel' step, so it looks like your application and not your Mini-ITX hardware.

     

    You have a lot of things going on here: the fsbl, u-boot, your OS, devicetree, bit stream etc. Is your zynq_fsbl current for your platform or did you copy it from somewhere else?

     

    You might want to check and see if your system will boot correctly with a simple bare-metal program with your PL loaded. Maybe one of the canned memory tests, peripheral tests or an echo test. Or you could write a simple bare-metal 'hello world' with an indication to the terminal that it is running and then load your bit stream to see if it does indeed crash the PS. This could indicate if the problem really is a bit stream that crashes the PS, a problem with your software, or some more complex interaction between the two.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cone83
    0 cone83 over 10 years ago in reply to e14 Contributor

    Hi Gary,

    Thank you so much for trying this out. Interesting to see that it got past the 3 second boot delay on another system. The whole thing actually boots nicely If I use a smaller bit stream. It also boots nicely if I use the large bit stream, but have all the logic idle. The system will then freeze immediately when the PL is put to work. On the external interfaces, there is no difference between the small and the large bit stream.

    I'll try chopping this design down even further. Maybe something is wrong with the constraints or the PS configuration. But I have used the original board definition files for these.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cone83
    0 cone83 over 10 years ago in reply to e14 Contributor

    Hi Gary,

    Thank you so much for trying this out. Interesting to see that it got past the 3 second boot delay on another system. The whole thing actually boots nicely If I use a smaller bit stream. It also boots nicely if I use the large bit stream, but have all the logic idle. The system will then freeze immediately when the PL is put to work. On the external interfaces, there is no difference between the small and the large bit stream.

    I'll try chopping this design down even further. Maybe something is wrong with the constraints or the PS configuration. But I have used the original board definition files for these.