Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PS freezes when making use of PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 356 subscribers
  • Views 3385 views
  • Users 0 members are here
Related

PS freezes when making use of PL

cone83
cone83 over 10 years ago

I am encountering very odd problems with my new Mini-ITX board. Whenever I make use of a significant portion of the PL resources, the PS just freezes.

I have done quite a lot of debugging on this, and the only thing that seems to affect this problem is the amount of resources used. I have a test design that does a lot of useless computations. If I allow Vivado to optimize away all the useless stuff and hence greatly reduce the resource usage, then the CPU does not freeze. If I prevent the optimization and use 56% LUTs, then the CPU freezes immediately.

There are no timing timing violations or other errors reported by Vivado. I have now come to a point where I suspect that my Zynq might actually be damaged.

I have created a set of boot files for reproducing this error on a Mini-ITX with Zynq 7100. The boot files can be downloaded here:
https://mega.nz/#F!9hF0kQrZ!RfGgoTnCO0QOtp6MSUFZxg

When booting this configuration, U-boot only manages to print a few lines on UART before the CPU stalls. Usually the output looks like this:

--------------
U-Boot 2015.07-dirty (Apr 09 2016 - 11:32:21 +0200)

Model: Zynq Mini-ITX Board
DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size
--------------

Sometimes it even freezes before being able to print the first line. I would be really thankful if somebody could try out those boot files and report if this error also occurs on other Mini-ITX boards with Zynq 7100 SoCs.

Many thanks

  • Sign in to reply
  • Cancel
Parents
  • cone83
    0 cone83 over 10 years ago

    I'm also not convinced yet that this isn't an issue with my board. Your test got stuck when loading the kernel. This could e.g. also be caused by a faulty device tree. To get sure  I have created a bare metal application for reproducing the fault. The application cycles between periods of low and high CPU loads, as I have found that some bit files work well for as long as the CPU is idle. On a functioning system, this should output something like this:

    Test with low CPU load
    0
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    Test with high CPU load
    0
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    Test with low CPU load
    0
    1
    ...

    For me it usually gets stuck after printing the first two lines. I have made the boot.bin file available at:
    https://mega.nz/#!QgtnRaAR!8QKhi_PFyIKuAeFEGoOdsmup8QKnQBcL6DoDhz6nPzI

    I would be really thankful if you or somebody else could give this another try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cone83
    0 cone83 over 10 years ago

    I'm also not convinced yet that this isn't an issue with my board. Your test got stuck when loading the kernel. This could e.g. also be caused by a faulty device tree. To get sure  I have created a bare metal application for reproducing the fault. The application cycles between periods of low and high CPU loads, as I have found that some bit files work well for as long as the CPU is idle. On a functioning system, this should output something like this:

    Test with low CPU load
    0
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    Test with high CPU load
    0
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    Test with low CPU load
    0
    1
    ...

    For me it usually gets stuck after printing the first two lines. I have made the boot.bin file available at:
    https://mega.nz/#!QgtnRaAR!8QKhi_PFyIKuAeFEGoOdsmup8QKnQBcL6DoDhz6nPzI

    I would be really thankful if you or somebody else could give this another try.