Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Working with i2c switch under Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 354 subscribers
  • Views 542 views
  • Users 0 members are here
Related

Working with i2c switch under Linux

e14 Contributor
e14 Contributor over 12 years ago

Hello everyone!

I have Ubuntu Linux launched on my MiniITX board and I'd like to write/read to i2c-eeprom.
In board User Guide it is said that jumper JP12 switches i2c-master. But there are no markers defining which position is current: 1-2 or 2-3. So I tried both and nothing changes in
# i2cdetect -l
output. It always says:
i2c-0   i2c     XILINX I2C at e0004000        I2C adapter
So as I understand, i2c master doesn't change. Is that o'k?

Also, I don't understand how to write to EEPROM through the i2c switch. I cannot find i2c addresses for the devices in documentation. As I understand, that EEPROM is empty and is not used by the system so there is no problem using it.

Thank you in advance.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

      JP12 allows you to select the mux control from either PS (1-2) or PL (2-3).  I don't have the latest production board so I'm not sure if the silkscreen has changed, but a little trick I learned is figure out which pin is #1 is to flip the board over and take a look at the solder mask underneath.  There will be one pin where the solder is in a square, and that indicates pin #1.   Not sure if that is universal, but it's true for all the Avnet boards.

    If you download the embedded design for the Mini-ITX from the Reference Design section, you will find an SDK project in the hierarchy.  For an example of using the EEPROM, take a look at the zynq_mini_itx_i2c_test project under that workspace.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    very much!