Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design FMC, AD9361
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 355 subscribers
  • Views 1557 views
  • Users 0 members are here
Related

FMC, AD9361

e14 Contributor
e14 Contributor over 10 years ago

Do the AD9361 boards (such as the AD-FMCOMMS3-EBZ), fit on the Zynq Mini-ITX FMC connector (can a LPC FMC connector plug into the HPC connector on the ITX board)?

If so, has anyone done this, and do you have a picture of the orientation?

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

     

    You can plug an LPC FMC into an HPC FMC connector, the HPC just has additional signals.

     

    The AD-FMCOMMS3-EBZ will fit on the Mini-ITX but the antennas may block the Zynq fansink on the Mini-ITX board. You may want to use SMA cables to connect to remote antennas. Here is a link to a picture of a Mini-ITX with an FMCCOMMS2 board installed:

     

    https://avnet.egnyte.com/dl/PMDkdq2g8n

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Perfect, Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi jclemmer,

    I have used the FMCCOMMS2 board installed on my Zynq Mini-ITX board with the use of an FMC Entender board which extends the height at which the FMC board is mounted relative to the mainboard:

    http://www.em.avnet.com/en-us/design/drc/Pages/Avnet-FMC-Extender.aspx

    Using this extender board, the antenna ports are no longer blocked by the fan/heatsink assembly.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Is this included in the base kit and the system kit, or what does it mean by "FMC Adapter" in the list of included items?

    Thanks,
    Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi,
    I use similar configuration, however, to limit the mechanical stress to the transceiver board I used SMA-SMA pigtails and moved the antennas to the rear panel of the box, see https://goo.gl/photos/mJviSZzWzKHrR3Jh9
    The FMCOMMS2/3 works well with mitx45, however according to AD support it should work with mitx100 as well, see https://ez.analog.com/message/246745#246745

    Rafal