Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PCIe problems when using USB 3.0 cards
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 355 subscribers
  • Views 4818 views
  • Users 0 members are here
Related

PCIe problems when using USB 3.0 cards

cone83
cone83 over 10 years ago

Hi,

I'm trying to get USB 3.0 running through the PCIe slot. I have been using two different USB 3.0 cards, one with a NEC and one with a VLI chip, but have experienced (different) problems with each. My hardware design very closely matches the PCIe reference design, and I'm running a small Linux system based on the Xilinx kernel v2015.4.01 (Linux 4.0.0).

The PCI bridge is correctly detected at boot, as is the USB PCIe card. USB devices that are plugged-in are detected and some actually seem to work without problems. I tested a USB 3.0 flash drive which seemed to work fine with both cards, and gets a read speed of 55 MB/s.

Problems seem to occur when I use devices with higher data rates. I have two different USB3 cameras from different manufacture. Both work well when connected to the USB2 ports, or to a USB3 port on a Linux PC. When connected to one of the PCIe cards I experience the following problems

NEC Card
========

For the first camera, reading and writing the camera settings work but when starting the image transfer I see the following errors:

usb 2-2: usbfs: process 9843 did not claim interface 2 before use
usb 2-1: usbfs: process 9843 did not claim interface 2 before use
xhci_hcd 0000:01:00.0: WARN Successful completion on short TX: needs XHCI_TRUST_TX_LENGTH quirk?

The other camera works when configured to small image sizes, but the frame rate drastically drops when transferring large images (like 1 frame per second)

VLI Card
========

The first camera doesn't work at all (not even reading / writing settings). No error is logged, only read-errors from the user space application.

The second camera again works well with small image sizes, but when configured to larger sizes, I receive USB disconnects and re-connects:

usb 2-2: USB disconnect, device number 5
usb 2-2: new SuperSpeed USB device number 8 using xhci_hcd
usb 2-2: New USB device found, idVendor=1409, idProduct=3240
usb 2-2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 2-2: Product: USB 3.0 Camera
usb 2-2: Manufacturer: Camera Manufacturer

======

So, I suppose there is a compatibility problem with the PCI-bridge and the USB3 cards when transferring high-bandwidth data. I receive some PCI errors during boot which might be related. Here are all PCI-related kernel messages:

xilinx-pcie 50000000.axi-pcie: PCIe Link is UP
PCI host bridge /amba/axi-pcie@50000000 ranges:
  No bus range found for /amba/axi-pcie@50000000, using [bus 00-ff]
  MEM 0x60000000..0x6fffffff -> 0x60000000
xilinx-pcie 50000000.axi-pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [bus 00-ff]
pci_bus 0000:00: root bus resource [mem 0x60000000-0x6fffffff]
PCI: bus0: Fast back to back transfers disabled
pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 0: no space for [mem size 0x40000000]
pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x40000000]
pci 0000:00:00.0: BAR 8: assigned [mem 0x60000000-0x600fffff]
pci 0000:01:00.0: BAR 0: assigned [mem 0x60000000-0x60001fff 64bit]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0:   bridge window [mem 0x60000000-0x600fffff]
pci 0000:00:00.0: enabling device (0140 -> 0142)
pci 0000:01:00.0: enabling device (0140 -> 0142)

I couldn't really fix the memory assignment error. However, the messages seem to match the logs posted by other users. For completion, the USB related messages are as follows:

xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 1
xhci_hcd 0000:01:00.0: hcc params 0x014051cf hci version 0x100 quirks 0x00000090
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: xHCI Host Controller
usb usb1: Manufacturer: Linux 4.0.0-xilinx xhci-hcd
usb usb1: SerialNumber: 0000:01:00.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 2 ports detected
xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: xHCI Host Controller
usb usb2: Manufacturer: Linux 4.0.0-xilinx xhci-hcd
usb usb2: SerialNumber: 0000:01:00.0
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 2 ports detected
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
usbcore: registered new interface driver usb-storage


Also, the relevant section of the device tree is as follows:

    pci_express: axi-pcie@50000000 {
        #address-cells = <3>;
        #size-cells = <2>;
        #interrupt-cells = <1>;
        compatible = "xlnx,axi-pcie-host-1.00.a";
        reg = < 0x50000000 0x04000000 >;
        device_type = "pci";
tinterrupts = < 0 33 4 >;
        interrupt-map-mask = <0 0 0 7>;
        interrupt-map = <0 0 0 1 &pcie_intc 1>,
                        <0 0 0 2 &pcie_intc 2>,
                        <0 0 0 3 &pcie_intc 3>,
                        <0 0 0 4 &pcie_intc 4>;
        ranges = < 0x02000000 0 0x60000000 0x60000000 0 0x10000000 >;
       
        pcie_intc: interrupt-controller {
             interrupt-controller;
             #address-cells = <0>;
             #interrupt-cells = <1>;
        };
    };

I know that the interrupt number is a bit odd, but that is correct (I have a few more things connected to IRQ_F2P). The interrupt is called, as I can see in /proc/interrupts.

I haven't yet tried any other PCIe cards, as I don't have any lying around. I'm really out of ideas on this problem by now. Any suggestions would be greatly welcome.

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    I am facing the same issue. Did you find some solution?

    My project involves two USB3.0 cameras. In order to handle the bandwidth I have a USB3.0 expansion card for the PCIe slot with 4 dedicated 5Gbps channels, the card is a x4 gen2 PCIe card. The card uses 4 Renesas chips.

    My Vivado design is similar to the reference design, I work on a Ubuntu 14.04 using the Vivado version 2016.1.

    The kernel version I use is the one from xilinx with the branch 2016.1.01 (version 4.4). The card gets enumerated correctly and each of the 4 ports work.

    When using a USB2.0 camera from the same vendor as the USB3.0 camera (same userspace drivers), I get correctly transferred data. But when using the USB3.0 camera with the higher speed, I get a transfer error. The communication seems to work, as I am able to control and setup the camera. Connecting the camera to a USB2.0 port works without any issues.

    I have also a "smaller" USB3.0 expansion card, which is a x1 gen2 PCIe with 2 ports but just one Renesas chip. This results in the same behavior, as with the "larger" card.

    I have also tested other branches until the latest master branch, still the version is 4.4, but the problem was the same.

    One thing I found out, that with the branch 2015.2.03, version 3.19, the "small" expansion card is working and I get correct data from the USB3.0 camera. The main issue with this kernel version is, that I cannot use the "larger" card, because the kernel somehow cannot handle the multiple Renesas chips on this card and during the boot, it hangs with the error message "xilinx-pcie 50000000.axi-pcie: Slave unsupported request".

    So basically in my case the transfer error on the USB3.0 occurs from the kernel version 4.0 and up. And interestingly the USB3.0 card with multiple Renesas chips is working only on kernel version 4.0 and up. Which leaves me with no working solution at this time.

    Any help or suggestion will be highly appreciated.

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    I am facing the same issue. Did you find some solution?

    My project involves two USB3.0 cameras. In order to handle the bandwidth I have a USB3.0 expansion card for the PCIe slot with 4 dedicated 5Gbps channels, the card is a x4 gen2 PCIe card. The card uses 4 Renesas chips.

    My Vivado design is similar to the reference design, I work on a Ubuntu 14.04 using the Vivado version 2016.1.

    The kernel version I use is the one from xilinx with the branch 2016.1.01 (version 4.4). The card gets enumerated correctly and each of the 4 ports work.

    When using a USB2.0 camera from the same vendor as the USB3.0 camera (same userspace drivers), I get correctly transferred data. But when using the USB3.0 camera with the higher speed, I get a transfer error. The communication seems to work, as I am able to control and setup the camera. Connecting the camera to a USB2.0 port works without any issues.

    I have also a "smaller" USB3.0 expansion card, which is a x1 gen2 PCIe with 2 ports but just one Renesas chip. This results in the same behavior, as with the "larger" card.

    I have also tested other branches until the latest master branch, still the version is 4.4, but the problem was the same.

    One thing I found out, that with the branch 2015.2.03, version 3.19, the "small" expansion card is working and I get correct data from the USB3.0 camera. The main issue with this kernel version is, that I cannot use the "larger" card, because the kernel somehow cannot handle the multiple Renesas chips on this card and during the boot, it hangs with the error message "xilinx-pcie 50000000.axi-pcie: Slave unsupported request".

    So basically in my case the transfer error on the USB3.0 occurs from the kernel version 4.0 and up. And interestingly the USB3.0 card with multiple Renesas chips is working only on kernel version 4.0 and up. Which leaves me with no working solution at this time.

    Any help or suggestion will be highly appreciated.

    Thanks!