Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PCIe problems when using USB 3.0 cards
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 355 subscribers
  • Views 4818 views
  • Users 0 members are here
Related

PCIe problems when using USB 3.0 cards

cone83
cone83 over 10 years ago

Hi,

I'm trying to get USB 3.0 running through the PCIe slot. I have been using two different USB 3.0 cards, one with a NEC and one with a VLI chip, but have experienced (different) problems with each. My hardware design very closely matches the PCIe reference design, and I'm running a small Linux system based on the Xilinx kernel v2015.4.01 (Linux 4.0.0).

The PCI bridge is correctly detected at boot, as is the USB PCIe card. USB devices that are plugged-in are detected and some actually seem to work without problems. I tested a USB 3.0 flash drive which seemed to work fine with both cards, and gets a read speed of 55 MB/s.

Problems seem to occur when I use devices with higher data rates. I have two different USB3 cameras from different manufacture. Both work well when connected to the USB2 ports, or to a USB3 port on a Linux PC. When connected to one of the PCIe cards I experience the following problems

NEC Card
========

For the first camera, reading and writing the camera settings work but when starting the image transfer I see the following errors:

usb 2-2: usbfs: process 9843 did not claim interface 2 before use
usb 2-1: usbfs: process 9843 did not claim interface 2 before use
xhci_hcd 0000:01:00.0: WARN Successful completion on short TX: needs XHCI_TRUST_TX_LENGTH quirk?

The other camera works when configured to small image sizes, but the frame rate drastically drops when transferring large images (like 1 frame per second)

VLI Card
========

The first camera doesn't work at all (not even reading / writing settings). No error is logged, only read-errors from the user space application.

The second camera again works well with small image sizes, but when configured to larger sizes, I receive USB disconnects and re-connects:

usb 2-2: USB disconnect, device number 5
usb 2-2: new SuperSpeed USB device number 8 using xhci_hcd
usb 2-2: New USB device found, idVendor=1409, idProduct=3240
usb 2-2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 2-2: Product: USB 3.0 Camera
usb 2-2: Manufacturer: Camera Manufacturer

======

So, I suppose there is a compatibility problem with the PCI-bridge and the USB3 cards when transferring high-bandwidth data. I receive some PCI errors during boot which might be related. Here are all PCI-related kernel messages:

xilinx-pcie 50000000.axi-pcie: PCIe Link is UP
PCI host bridge /amba/axi-pcie@50000000 ranges:
  No bus range found for /amba/axi-pcie@50000000, using [bus 00-ff]
  MEM 0x60000000..0x6fffffff -> 0x60000000
xilinx-pcie 50000000.axi-pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [bus 00-ff]
pci_bus 0000:00: root bus resource [mem 0x60000000-0x6fffffff]
PCI: bus0: Fast back to back transfers disabled
pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 0: no space for [mem size 0x40000000]
pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x40000000]
pci 0000:00:00.0: BAR 8: assigned [mem 0x60000000-0x600fffff]
pci 0000:01:00.0: BAR 0: assigned [mem 0x60000000-0x60001fff 64bit]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0:   bridge window [mem 0x60000000-0x600fffff]
pci 0000:00:00.0: enabling device (0140 -> 0142)
pci 0000:01:00.0: enabling device (0140 -> 0142)

I couldn't really fix the memory assignment error. However, the messages seem to match the logs posted by other users. For completion, the USB related messages are as follows:

xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 1
xhci_hcd 0000:01:00.0: hcc params 0x014051cf hci version 0x100 quirks 0x00000090
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: xHCI Host Controller
usb usb1: Manufacturer: Linux 4.0.0-xilinx xhci-hcd
usb usb1: SerialNumber: 0000:01:00.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 2 ports detected
xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: xHCI Host Controller
usb usb2: Manufacturer: Linux 4.0.0-xilinx xhci-hcd
usb usb2: SerialNumber: 0000:01:00.0
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 2 ports detected
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
usbcore: registered new interface driver usb-storage


Also, the relevant section of the device tree is as follows:

    pci_express: axi-pcie@50000000 {
        #address-cells = <3>;
        #size-cells = <2>;
        #interrupt-cells = <1>;
        compatible = "xlnx,axi-pcie-host-1.00.a";
        reg = < 0x50000000 0x04000000 >;
        device_type = "pci";
tinterrupts = < 0 33 4 >;
        interrupt-map-mask = <0 0 0 7>;
        interrupt-map = <0 0 0 1 &pcie_intc 1>,
                        <0 0 0 2 &pcie_intc 2>,
                        <0 0 0 3 &pcie_intc 3>,
                        <0 0 0 4 &pcie_intc 4>;
        ranges = < 0x02000000 0 0x60000000 0x60000000 0 0x10000000 >;
       
        pcie_intc: interrupt-controller {
             interrupt-controller;
             #address-cells = <0>;
             #interrupt-cells = <1>;
        };
    };

I know that the interrupt number is a bit odd, but that is correct (I have a few more things connected to IRQ_F2P). The interrupt is called, as I can see in /proc/interrupts.

I haven't yet tried any other PCIe cards, as I don't have any lying around. I'm really out of ideas on this problem by now. Any suggestions would be greatly welcome.

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Have you configured the PCIe core for Gen 1 or Gen 2?

     

    If Gen 1 then you might want to try configuring for Gen 2.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Have you configured the PCIe core for Gen 1 or Gen 2?

     

    If Gen 1 then you might want to try configuring for Gen 2.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • cone83
    0 cone83 over 10 years ago in reply to e14 Contributor

    Hi Gary!

    I suppose with Gen2 you mean setting a link speed of 5 GT/s in the IP block? I have actually tried both settings, but didn't notice a difference either way.