Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PS not responding
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 354 subscribers
  • Views 590 views
  • Users 0 members are here
Related

PS not responding

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I am trying to run a simple helloworld+led-blink application on the Mini-ITX. I have tried JTAG, QSPI, and SD Card configuration, with varying results.

Using JTAG, I am able to program the PL, but the PS does not print "hello world" over UART, and the GPIO-controlled LEDs do not blink.

Using QSPI, the PL never gets programmed and the PS also does not run my helloworld app.

Using SD Card, the PL gets programmed, but the PS does not run my helloworld app.

Everything works perfect when I program the Mini-ITX with the provided .mcs and .bit files from the "zynq_mini_itx_7z045_embedded_design_v2015_2" project.

Furthermore, I can successfully run a helloworld app on the standard Zedboard, but not on my Mini-ITX board.

I can't figure out why the Zedboard works fine but the Mini-ITX is having this problem. For each of these boards, I have used the correct board files and constraint files. I am running Vivado 2015.4.

Can anybody provide some troubleshooting steps I can take?

Thank you

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

     

    The fact that the provided .mcs and .bit files work seem to confirm that your hardware is working OK. I assume that you were able to see output on the serial terminal with these files.

     

    At this point I would guess that it is one of two things. Either your Vivado installation is corrupted and the project you have generated is flawed or, more likely, you have used the wrong board configuration file. Can you check and see if the MD5 checksum for the Vivado installation file you downloaded matches the one published on the Xilinx download site? If not I would suggest removing and re-installing Vivado. These corrupt installations are rare but do happen and can cause strange results.

     

    If the Vivado MD5 checksum is good then please make sure that you have downloaded and installed the correct Mini-ITX board files, the ones labeled "2015.3 or later" from the Mini-ITX documents page:

     http://zedboard.org/support/documentation/2056

     

    Then I would try to generate your Vivado design and export to the SDK. Then build the hello world app and try again. You might also want to try a 'new' location for the SDK workspace as, occasionally, the SDK does not update with a new hardware design as expected. You could also force an update in the SDK.

     

    The only other thing I can think to try would be to run your 'hello world' application from the SDK debugger and see if it connects and comes up properly. If not that probably points back to the wrong board files.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary,

    Thanks for your suggestions.

    I updated to 2015.4, verified that the MD5 checksums matched, regenerated and rebuilt everything, and the issues remained.

    I verified that I was using the correct board files as well.

    Then, I downloaded and installed 2015.3, and verified that the MD5 checksums matched. After rebuilding everything from scratch, again with the correct board files, and then creating a new SDK project, I still saw the same issues.

    Running the app with SDK debugger also does not help.

    What else can I check or do? By the way, I am able to connect to the PS through XMD, write to the LEDgpio addresses, and control the LEDs.

    Thank you