Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design mini-itx DDR problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 355 subscribers
  • Views 1489 views
  • Users 0 members are here
Related

mini-itx DDR problem

jenn.holt
jenn.holt over 10 years ago

I recently purchased a mini-itx100 system and am having trouble getting it to boot. None of the pre-packaged designs seemed to word(sd card or qspi flash), but the JTAG connection works ok, so I tried building some of the reference designs.

So far the only one that works somewhat is the 'zynq_mini_itx_mem_test' part of the embedded design. This code will partially run, but it hangs any time it tries to run the DDR tests (either the PS or PL one). If I modify the code to exclude those tests, the ps7_ram test passes.

I suspect that the problem is with my DDR ram, or its configuration, since the mem_test code is not loaded in to DDR ram, and it runs fine as long as it doesn't try to access any DDR. 

I read that the newer boards have different RAM chips, (mine is revision E) but that they are not supposed to require any software changes.

Does anyone have any idea of what tests I can run to narrow down the problem?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Jenn.holt,

    First I would like for you to double check that you set up your Mini-ITX properly. Go to the "Getting Started Guide" at http://zedboard.org/support/documentation/2056 and go to the "Setting up the Board" section and double check your setup. If that all checks out, check the power module and make sure it is tighly seated and the mounting screws are installed. Then check all power module voltage rails on your Mini-ITX board(we have test point and an LED for each rail) to make sure all the rails are OK.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jenn.holt
    0 jenn.holt over 10 years ago in reply to jafoste4

    So I checked the setup, and that was OK, but there is a problem with the power supply. Test point 5 for the 1.5/1.35V rail only reads 0.6V. This is enough to weakly light the LED, so I missed it the first time around.

    I checked the corresponding pin on the power supply module to rule out a bad connection, and it also reads 0.6V.

    Will it damage the power supply module if I take it off and power it up unloaded?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jenn.holt
    0 jenn.holt over 10 years ago in reply to jenn.holt

    I noticed one other thing, which is probably the whole problem. The power supply module has a jumper to select 1.5/1.35V and there is no jumper installed. Which voltage is appropriate for the board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jenn.holt
    0 jenn.holt over 10 years ago in reply to jenn.holt

    I noticed one other thing, which is probably the whole problem. The power supply module has a jumper to select 1.5/1.35V and there is no jumper installed. Which voltage is appropriate for the board?