Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design How to connect the 2 leds in the same axi gpio interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 1597 views
  • Users 0 members are here
Related

How to connect the 2 leds in the same axi gpio interface

innodim
innodim over 9 years ago

MiniZed board has two pl leds (green and blue). In the IP integrator block diagram (vivado 2017.1) I can create an axi gpio interface and automatically connect one of the the two leds. Given that GPIO interface supports up to 32 bits it seems too much to use a second channel or a second axi gpio interface for connecting the second led. I can customise the axi gpio channel to support 2 bits but then how to connect the automatically inferred gpio_rtl signal to the leds? Graphically it doesn't seem possible. I suspect I have to use a custom constraint file but I am clueless about where leds map to the fpga

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello InnoDim,

    We have an example design on our reference design page that accesses the two PL leds using a single axi gpio and then routes it through the PL using constratins. My suggestion for you would be to use this is an example as you create your project.

    Please refer to the refernece design "Prebuilt Platforms Using Hardware Definition Files(HDFs)" It goes through the process of using automated build scripts to build the project, after you build it you will be able to open it an explore it, leverage it in your design.

    http://minized.org/support/design/18891/146

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • innodim
    0 innodim over 9 years ago in reply to jafoste4

    Thank you Josh, that was helpful

    Although as seen from the block design the two leds are connected to two channels of the same gpio I was able to retrieve the mapping between leds and package pins in the constraint files. For those who wonder these are package pin E12 ->red led and package pin E13 -> green led. So I was able to create a custom 2-bit signal connected in a single channel of one gpio and assign it via an xdc file the leds with it.

    It would be useful (if not necessary) avnet to include in the minized hardware user guide all the mappings between board leds, buttons, arduino pins, pmod pins with the package pins of fpga, or provide a reference xdc file with comments of the mappings, instead of digging in that reference design or the other

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • innodim
    0 innodim over 9 years ago in reply to jafoste4

    Thank you Josh, that was helpful

    Although as seen from the block design the two leds are connected to two channels of the same gpio I was able to retrieve the mapping between leds and package pins in the constraint files. For those who wonder these are package pin E12 ->red led and package pin E13 -> green led. So I was able to create a custom 2-bit signal connected in a single channel of one gpio and assign it via an xdc file the leds with it.

    It would be useful (if not necessary) avnet to include in the minized hardware user guide all the mappings between board leds, buttons, arduino pins, pmod pins with the package pins of fpga, or provide a reference xdc file with comments of the mappings, instead of digging in that reference design or the other