Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Bitstream Generation Fail
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 3750 views
  • Users 0 members are here
Related

Bitstream Generation Fail

chchyong89
chchyong89 over 8 years ago

Hi all

I am using minized for this test but i am having error when generating bitstream. 

Here is the vhdl code i taken from the internet:

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
 
entity clk200Hz is
    Port (
        clk_in : in  STD_LOGIC;
        reset  : in  STD_LOGIC;
        clk_out: out STD_LOGIC
    );
end clk200Hz;
 
architecture Behavioral of clk200Hz is
    signal temporal: STD_LOGIC;
    signal counter : integer range 0 to 4999 := 0;
begin
    frequency_divider: process (reset, clk_in) begin
        if (reset = '1') then
            temporal <= '0';
            counter <= 0;
        elsif rising_edge(clk_in) then
            if (counter = 4999) then
                temporal <= NOT(temporal);
                counter <= 0;
            else
                counter <= counter + 1;
            end if;
        end if;
    end process;
    
    clk_out <= temporal;
end Behavioral;

 

Below is my xdc

      set_property  PACKAGE_PIN C7  [get_ports clk_in]
        set_property  IOSTANDARD LVCMOS33  [get_ports clk_in]
        create_clock -name clkin  -period 30.00  [get_ports clk_in]
      set_property  PACKAGE_PIN D8  [get_ports reset]
        set_property  IOSTANDARD LVCMOS33  [get_ports reset]
      set_property  PACKAGE_PIN C13  [get_ports clk_out]
        set_property  IOSTANDARD LVCMOS33  [get_ports clk_out]
 
 
 
and here is the error:
  [DRC UCIO-1] Unconstrained Logical Port: 3 out of 3 logical ports have no user assigned specific location constraint (LOC). This may cause I/O contention or incompatibility with the board power or connectivity affecting performance, signal integrity or in extreme cases cause damage to the device or the components to which it is connected. To correct this violation, specify all pin locations. This design will fail to generate a bitstream unless all logical ports have a user specified site LOC constraint defined.  To allow bitstream creation with unspecified pin locations (not recommended), use this command: set_property SEVERITY {Warning} [get_drc_checks UCIO-1].  NOTE: When using the Vivado Runs infrastructure (e.g. launch_runs Tcl command), add this command to a .tcl file and add that file as a pre-hook for write_bitstream step for the implementation run.  Problem ports: clk_in, clk_out, and reset.
   
 
 
  • Sign in to reply
  • Cancel
Parents
  • chchyong89
    0 chchyong89 over 8 years ago
    I have check through the implementation log, seems like it cannot access to the "site location" ? 
     
      CRITICAL WARNING: [Vivado 12-1411] Cannot set LOC property of ports, Site location is not valid [C:/Xilinx/VHDLProject/Test2/project_1/project_1.srcs/constrs_1/new/PWM.xdc:5]
      CRITICAL WARNING: [Vivado 12-1411] Cannot set LOC property of ports, Site location is not valid [C:/Xilinx/VHDLProject/Test2/project_1/project_1.srcs/constrs_1/new/PWM.xdc:7]
      CRITICAL WARNING: [Vivado 12-1411] Cannot set LOC property of ports, Site location is not valid [C:/Xilinx/VHDLProject/Test2/project_1/project_1.srcs/constrs_1/new/PWM.xdc:9]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • chchyong89
    0 chchyong89 over 8 years ago
    I have check through the implementation log, seems like it cannot access to the "site location" ? 
     
      CRITICAL WARNING: [Vivado 12-1411] Cannot set LOC property of ports, Site location is not valid [C:/Xilinx/VHDLProject/Test2/project_1/project_1.srcs/constrs_1/new/PWM.xdc:5]
      CRITICAL WARNING: [Vivado 12-1411] Cannot set LOC property of ports, Site location is not valid [C:/Xilinx/VHDLProject/Test2/project_1/project_1.srcs/constrs_1/new/PWM.xdc:7]
      CRITICAL WARNING: [Vivado 12-1411] Cannot set LOC property of ports, Site location is not valid [C:/Xilinx/VHDLProject/Test2/project_1/project_1.srcs/constrs_1/new/PWM.xdc:9]