Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design pmods in minized board files
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 3668 views
  • Users 0 members are here
Related

pmods in minized board files

sgawad
sgawad over 8 years ago

Hello all,

 

I am trying to add Pmods to my board diagram.

I wonder why they don't show up in the "Board" tab.

I do see the 2 leds (pl_led_r and pl_led_g)

as well as (pl_sw_1bit) 

But the pmod ports don't show up. (Although they maybe should based on the digilent tutorial I follow for an other board)

Also I run the tcl for the speedway but after it's done (successfully) when I go to project settings the project device is not a board but rather just the chip. Is that intended?

 

Thank you in advance and sorry to ask those naive questions.

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 8 years ago +1 verified
    Hi Shady, Digilent has their pmods listed in the boards tab due to in the board definition file they use. I'm not sure exactly how, but i believe some flag is set off in that file to indicate the Pmod…
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi Shady,

    Digilent has their pmods listed in the boards tab due to in the board definition file they use. I'm not sure exactly how, but i believe some flag is set off in that file to indicate the Pmod interfaces. Or it could be information taken from the vivado-library they have you install.

    A master constraint file is available for the MiniZed located here http://zedboard.org/support/documentation/18891 It has the Pmod constraints your looking for.

    The warnings are most likely vivado complaining about some timing issue. Due to the low speeds running on the MiniZed these can be ignored. 

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi Shady,

    Digilent has their pmods listed in the boards tab due to in the board definition file they use. I'm not sure exactly how, but i believe some flag is set off in that file to indicate the Pmod interfaces. Or it could be information taken from the vivado-library they have you install.

    A master constraint file is available for the MiniZed located here http://zedboard.org/support/documentation/18891 It has the Pmod constraints your looking for.

    The warnings are most likely vivado complaining about some timing issue. Due to the low speeds running on the MiniZed these can be ignored. 

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer