Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design How to re-create .bin and .elf file?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 986 views
  • Users 0 members are here
Related

How to re-create .bin and .elf file?

hs15
hs15 over 8 years ago

Hello everyone,

I've re-created the "Python Web Server on MiniZed" hardware project by sourcing the "make_minized_petalinux.tcl" in Vivado. Now, I'm trying change a few things in the hardware block design and re-create the corresponding .bin and .elf and program the board through xsct. 

Can someone please help me with this?

  • Sign in to reply
  • Cancel
Parents
  • hs15
    0 hs15 over 8 years ago

    Thank you for your response. Yes, I've done all of those. Is HDF the only file that I should replace compared to the previous project? How about .bit and .dtb?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago in reply to hs15

    The HDF file is like a special zip file and it includes the .bit file that Vivado generated.  When you import the HDF with the command given above, PetaLinux takes it as part of the dts/dti file inputs for the device tree.  As part of the build process, a dts file is compiled to be a dtb file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hs15
    0 hs15 over 8 years ago in reply to stefanrousseau

    Thanks for your response. So, I don't need to recreate the device tree in sdk, the new device tree containing new modified physical addresses and etc will be included by importing HDF file? 

    I have another question: When I build the new Petalinux (including new hardware architecture) and run it on the board, how can I check in Petalinux's terminal whether the defined AXI master/slave ports are included or not (whether the new hardware design is reflected in Petalinux)? How to check the corresponding physical addresses too? For example, if I add two more GPIO via AXI_GP.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hs15
    0 hs15 over 8 years ago in reply to stefanrousseau

    Thanks for your response. So, I don't need to recreate the device tree in sdk, the new device tree containing new modified physical addresses and etc will be included by importing HDF file? 

    I have another question: When I build the new Petalinux (including new hardware architecture) and run it on the board, how can I check in Petalinux's terminal whether the defined AXI master/slave ports are included or not (whether the new hardware design is reflected in Petalinux)? How to check the corresponding physical addresses too? For example, if I add two more GPIO via AXI_GP.

     

    Thanks!