Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Trouble building PetaLinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 360 subscribers
  • Views 3258 views
  • Users 0 members are here
Related

Trouble building PetaLinux

chrisp_002
chrisp_002 over 8 years ago

Hi all,

 

Currently trying to get to grips with the MiniZed. Trying to get my head around how PetaLinux and Vivado are used in order to work towards bespoke utilization of the Zynq7000S.

 

At the moment I am trying to create build a new PetaLinux system image, after having modified the Kernel configuration to include additional drivers I need for my application. I have used the following process so far, executed in the order described below..

 

Downloaded the BSP..

'Creating a PetaLinux 2017.2 BSP used for Booting from QSPI and eMMC'

Sucessfully created a new PetaLinux project using the .bsp file included.

Used 'petalinux-config --get-hw-description' to reference the HDF file included in the aformentioned BSP package download.

Used 'petalinux-config -c kernel' to add additional drivers required for my project.

Used 'petalinux-build' to build a new system image.

 

As far as I know, I am executing the steps above in the correct order. However, during the petalinux-build I am getting errors.

The log containing the first error reads as follows..

 

EBUG: Executing python function sysroot_cleansstate
DEBUG: Python function sysroot_cleansstate finished
DEBUG: Executing shell function do_configure
MISC_ARG is  -yamlconf /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/device-tree-generation.yaml
APP_ARG is  -app "device-tree"
cmd is: xsct /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/dtgen.tcl -ws /home/chrisp/TestProj/build/../components/plnx_workspace/device-tree -pname device-tree-generation -rp /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/git -processor ps7_cortexa9_0 -hdf /home/chrisp/TestProj/deploy/images/plnx_arm/Xilinx-plnx_arm.hdf -arch 32  -app "device-tree"  -yamlconf /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/device-tree-generation.yaml
CRITICAL WARNING: [Board 49-71] The board_part definition was not found for em.avnet.com:minized:part0:1.2. The project's board_part property was not set, but the project's part property was set to xc7z007sclg225-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.
INFO: [Hsi 55-1698] elapsed time for repository loading 0 seconds
ERROR: [Common 17-55] 'get_property' expects at least one object.
Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.
ERROR: [Hsi 55-1545] Problem running tcl command ::sw_device_tree::post_generate : ERROR: [Common 17-55] 'get_property' expects at least one object.
Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.

    while executing
"get_property IP_NAME [get_cells -hier $proc_name]"
    (procedure "update_cpu_node" line 23)
    invoked from within
"update_cpu_node $os_handle"
    (procedure "::sw_device_tree::post_generate" line 4)
    invoked from within
"::sw_device_tree::post_generate device_tree"
ERROR: [Hsi 55-1443] Error(s) while running TCL procedure post_generate()
generate_target failed
    while executing
"error "generate_target failed""
    invoked from within
"if {[catch {hsi generate_target -dir $project} res]} {
    error "generate_target failed"
}"
    (file "/home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/dtgen.tcl" line 33)
WARNING: /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/temp/run.do_configure.25053:1 exit 1 from 'eval xsct /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/dtgen.tcl -ws /home/chrisp/TestProj/build/../components/plnx_workspace/device-tree -pname device-tree-generation -rp /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/git -processor ps7_cortexa9_0 -hdf /home/chrisp/TestProj/deploy/images/plnx_arm/Xilinx-plnx_arm.hdf -arch 32 ${APP_ARG} ${MISC_ARG}'
ERROR: Function failed: do_configure (log file is located at /home/chrisp/TestProj/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+3c7407f6f8-r0/temp/log.do_configure.25053)

 

Although I am working toward a solution, I am currently unable to resolve this issue. Any help would be greatly appriciated.

 

Cheers,

Chris.

  • Sign in to reply
  • Cancel
  • chrisp_002
    0 chrisp_002 over 8 years ago

    FYI, I am using PetaLinux 2017.4 (and also have Vivado 2017.4 installed)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi Chris,

    Have you taken a look at our integrating Sensors on MiniZed with Petalinux Speedway?

    http://zedboard.org/support/trainings-and-videos

    Thats where I would start.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisp_002
    0 chrisp_002 over 8 years ago in reply to jafoste4

    Had a look through it, didn't help an awful lot.. though I feel I'm slowly starting to pickup a bit more on the overall process. 

    I think most of the problem is due to lack of a guide that goes from scratch through to an implemtented Petalinux system. All the guides I have found seem to gloss over different parts of the process, prompting the user to download and use pre-provided files.

    One document, detailing a from-scratch to a bootable petalinux system, using no pre-provided files would be far more helpful than wading through all available documentation, trying to piece it together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 8 years ago

    Chris,

    There are WIKI entries on Xilinx's with that level of detail with their kits and the above linked Tutorial is a generate from scratch tutorial.  When scripting is provided in Avnet tutorials, it is there to allow a user to pick and choose the amount of detail they want to go through. 

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisp_002
    0 chrisp_002 over 8 years ago in reply to drozwood90

    I'll give it all a look, and try going through that tutorial again. I think maybe I need to dig into the material a bit more by the sound of it.

     

    Cheers,

    Chris.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisp_002
    0 chrisp_002 over 8 years ago

    Well, turns out it was never gonna work.

    Apparently in 2017.3/4 device tree generation doesn't build for single-core zynq devices, pretty big deal really. 

    A patch was required.. https://www.xilinx.com/support/answers/70402.html

    Petalinux is building fine now. 

    Chris.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • jotuskuo
    0 jotuskuo over 8 years ago

    Hi,

    I use petalinux-v2017.2 to build project as following command line.

    a. petalinux-create -t project --template zynq --name dacTest
    b. cd dacTest
    c. petalinux-config --get-hw-description=/mnt/shared/DAC
    d. petalinux-build
     
    But one error occurs as following.
     
      [INFO] generating kernel configuration files
      [INFO] generating kconfig for Rootfs
      Generate rootfs kconfig
      [INFO] oldconfig rootfs
      [INFO] generating petalinux-user-image.bb
      INFO: bitbake petalinux-user-image
      Loading cache: 100% |###################################################################################################################################################################################################| Time: 0:00:01
      Loaded 3235 entries from dependency cache.
      Parsing recipes: 100% |#################################################################################################################################################################################################| Time: 0:00:04
      Parsing of 2446 .bb files complete (2410 cached, 36 parsed). 3236 targets, 224 skipped, 0 masked, 0 errors.
      NOTE: Resolving any missing task queue dependencies
      Initialising tasks: 100% |##############################################################################################################################################################################################| Time: 0:01:01
      Checking sstate mirror object availability: 100% |######################################################################################################################################################################| Time: 0:00:21
      NOTE: Executing SetScene Tasks
      NOTE: Executing RunQueue Tasks
      ERROR: device-tree-generation-xilinx+gitAUTOINC+43551819a1-r0 do_configure: Function failed: do_configure (log file is located at /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/temp/log.do_configure.9199)
      ERROR: Logfile of failure stored in: /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/temp/log.do_configure.9199
      Log data follows:
      | DEBUG: Executing python function sysroot_cleansstate
      | DEBUG: Python function sysroot_cleansstate finished
      | DEBUG: Executing shell function do_configure
      | MISC_ARG is  -yamlconf /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/device-tree-generation.yaml
      | APP_ARG is  -app "device-tree"
      | cmd is: xsct /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/dtgen.tcl -ws /home/jotus/work/petalinux/DacProj/build/../components/plnx_workspace -pname device-tree-generation -rp /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/git -processor ps7_cortexa9_0 -hdf /home/jotus/work/petalinux/DacProj/build/tmp/deploy/images/plnx_arm/Xilinx-plnx_arm.hdf -arch 32  -app "device-tree"  -yamlconf /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/device-tree-generation.yaml
      | INFO: [Hsi 55-1698] elapsed time for repository loading 0 seconds
      | ERROR: [Common 17-55] 'get_property' expects at least one object.
      | Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.
      | ERROR: [Hsi 55-1545] Problem running tcl command ::sw_device_tree::generate : ERROR: [Common 17-55] 'get_property' expects at least one object.
      | Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.
      | 
      |     while executing
      | "common::get_property IP_NAME $sink_periph"
      |     ("foreach" body line 8)
      |     invoked from within
      | "foreach intr_sink ${intr_sink_pins} {
      |               set sink_periph [::hsi::get_cells -of_objects $intr_sink]
      |               if { [llength $sink_periph ] && [::hsi::utils::is_..."
      |     (procedure "get_intr_cntrl_name" line 38)
      |     invoked from within
      | "get_intr_cntrl_name $drv_handle $pin"
      |     ("foreach" body line 2)
      |     invoked from within
      | "foreach pin ${intr_port_name} {
      |               set connected_intc [get_intr_cntrl_name $drv_handle $pin]
      |               if {[llength $connected_intc] == 0 } {
      |                       dtg_warning "I..."
      |     (procedure "gen_interrupt_property" line 18)
      |     invoked from within
      | "gen_interrupt_property $drv_handle"
      |     ("foreach" body line 7)
      |     invoked from within
      | "foreach drv_handle [get_drivers] {
      |         # generate the default properties
      |         gen_peripheral_nodes $drv_handle "create_node_only"
      |         gen_r..."
      |     (procedure "::sw_device_tree::generate" line 3)
      |     invoked from within
      | "::sw_device_tree::generate device_tree"
      | ERROR: [Hsi 55-1442] Error(s) while running TCL procedure generate()
      | generate_target failed
      |     while executing
      | "error "generate_target failed""
      |     invoked from within
      | "if {[catch {hsi generate_target -dir $project} res]} {
      |       error "generate_target failed"
      | }"
      |     (file "/home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/dtgen.tcl" line 33)
      | WARNING: /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/temp/run.do_configure.9199:1 exit 1 from 'eval xsct /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/dtgen.tcl -ws /home/jotus/work/petalinux/DacProj/build/../components/plnx_workspace -pname device-tree-generation -rp /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/git -processor ps7_cortexa9_0 -hdf /home/jotus/work/petalinux/DacProj/build/tmp/deploy/images/plnx_arm/Xilinx-plnx_arm.hdf -arch 32 ${APP_ARG} ${MISC_ARG}'
      | ERROR: Function failed: do_configure (log file is located at /home/jotus/work/petalinux/DacProj/build/tmp/work/plnx_arm-xilinx-linux-gnueabi/device-tree-generation/xilinx+gitAUTOINC+43551819a1-r0/temp/log.do_configure.9199)
      ERROR: Task (/home/jotus/work/petalinux/components/yocto/source/arm/layers/meta-xilinx-tools/recipes-bsp/device-tree/device-tree-generation_git.bb:do_configure) failed with exit code '1'
      NOTE: Tasks Summary: Attempted 2329 tasks of which 1865 didn't need to be rerun and 1 failed.
       
      Summary: 1 task failed:
        /home/jotus/work/petalinux/components/yocto/source/arm/layers/meta-xilinx-tools/recipes-bsp/device-tree/device-tree-generation_git.bb:do_configure
      Summary: There was 1 ERROR message shown, returning a non-zero exit code.
      ERROR: Failed to build project
       
       

    Any solution will be grateful.

    BTW, how to attach my hdf file? I doubt my hdf file is the problem.