Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed Development Process Help
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1695 views
  • Users 0 members are here
  • petalinux
  • minized
Related

MiniZed Development Process Help

dlux
dlux over 7 years ago

Hello,

 

I would like some help determining the development process for the MiniZed. Essentially, I am trying to create my own custom verilog code as well as C code, while still having petalinux and WiFi functionality. Currently I am trying my best to follow the "Integrating Sensors on MiniZed with PetaLinux (2017.1 and 2017.4)" tutorial. My problem with this tutorial is that too many of the files are pre-generated. Specifically, LAB1 shows how to create a boot.bin file for QSPI programming and then LAB2 shows how to program the image.ub into the emmc, but it also includes a bootemmc.bin file. As far as I understand, the bootemmc.bin file is also reprogramming the QSPI flash. Is there is difference between boot.bin of LAB1 and bootemmc.bin of LAB2? Maybe I am missing something, but I cannot seem to find how to generate the bootemmc.bin file. How is this possible?

 

I would like to generate a base project where I can develop my own PL and PS code. What I have tried so far:

 

1. Generate a project using petalinux-create using the bsp "MiniZed.bsp 2018.2 (BSP for booting from QSPI flash to eMMC)"

2. When I open the Vivado project created by this command the following files are missing:

     a) wireless_mgr.vhd

     b) minized_LEDs.xdc

     c) bitstream_compression_enable.xdc

     d) minized_petalinux.xdc

3. I found these missing files at https://github.com/Avnet/hdl and inserted them where Vivado was looking for them. Why is this necessary or how do I handle this properly?

4. Bit stream in Vivado was then successfully generated. Now I know I could edit the hardware design and it would successfully generate the bit and hdf files.

5. Exported the necessary HDF from Vivado and ran petalinux-config using the newly generated .hdf file

6. Exited the "Xilinx PetaLinux configuration editor" without changing anything

7. Ran petalinux-build

8. Now this is where some confusion comes into play:

     a) the petalinux-build command generated a boot.bin file without running boot_gen.sh! So, I tried programming this boot.bin file using "exec program_flash -f boot.bin -fsbl zynq_fsbl.elf -flash_type qspi_single" (on Windows). The "zynq_fsbl.elf" was also taken from the generated files from petalinux-build. This messed up the system enough that I got error "Zynq> ERROR: [Xicom 50-186] Error while detecting SPI flash device - unrecognized JEDEC id bytes: 00, 00, 00" when trying to follow "Restoring MiniZed to the Factory State" using XSCT (on Windows). I had to use the "Programming the QSPI Flash from the Vivado Hardware Manager" section of that file to get it back to normal (again on Windows).

     b) I adapted the boot_gen.sh script to work with my project. I thought maybe the starting addresses were incorrect in the boot.bin file generated purely from petalinux-build. In this case when using the Vivado Hardware Manager on Windows to program the flash using this boot.bit file, I get the error. "ERROR: [Labtools 27-3347] Flash Programming Unsuccessful: Program File Size cannot be greater than flash part size".

     c) I have not tried using petalinux-package as this was not used in any of Avnet's documentation (besides generating BSPs, from what I've seen).

 

This is my current attempt and thought process. I will follow LAB6 of "Integrating Sensors on MiniZed with PetaLinux (2017.1 and 2017.4)" to add my own C application, once I get there. For now, I want to to be able to generate the bootemmc.bin and image.ub files for a QSPI and eMMC build using the "MiniZed.bsp 2018.2 (BSP for booting from QSPI flash to eMMC)" as a basis. I am unsure if I am going about this correctly. Feel free to give me any suggestions and pointers you seem necessary.

 

Furthermore, running any of the MiniZed scripts at https://github.com/Avnet/hdl does nothing on both Windows and linux.

 

I am running Vivado 2018.2 on WIndows 10

I used the prebuilt virtual box image file for Ubuntu 16.04. I had to update some files to properly run Vivado/SDK 2018.2. I also installed petalinux 2018.2 tools.

 

Thanks for your help,

Richard

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 7 years ago +1
    I can't help you with specifics, but I found the following to be great resources when getting to grips with the Zynq. The Avnet Speedway Workshops are pretty much the same as the Path to Programmable challenge…
Parents
  • Fred27
    0 Fred27 over 7 years ago

    I can't help you with specifics, but I found the following to be great resources when getting to grips with the Zynq.

     

    The Avnet Speedway Workshops are pretty much the same as the Path to Programmable challenge that was recently featured here. The course is listed on zedboard.org (although you will need to register).

    http://zedboard.org/course/developing-zynq-hardware-vivado-20171-and-20174

     

    I also found that The Zynq Book is a great book - and free as a PDF.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Fred27
    0 Fred27 over 7 years ago

    I can't help you with specifics, but I found the following to be great resources when getting to grips with the Zynq.

     

    The Avnet Speedway Workshops are pretty much the same as the Path to Programmable challenge that was recently featured here. The course is listed on zedboard.org (although you will need to register).

    http://zedboard.org/course/developing-zynq-hardware-vivado-20171-and-20174

     

    I also found that The Zynq Book is a great book - and free as a PDF.