Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed PL LED Constraints
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 1728 views
  • Users 0 members are here
Related

MiniZed PL LED Constraints

armaank
armaank over 5 years ago

I am having trouble connecting external I/O components to the ARJ2 connector. I want to use the AD3, AD4, and AD5 pins which respectively translate to E13, E12, and E11 Zynq package pins. However, I am aware that these pins are used for the PL LEDs and PL switch. I am not sure how to disable the PL I/O so that when I send a signal to these 3 pins, it goes to my externally connected I/O rather than the PL I/O. I am programming the MiniZed using Verilog in Vivado 2020.1.1. Any help would be greatly appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • stefanrousseau
    stefanrousseau over 5 years ago +1 verified
    AD3, AD4 and AD5 are indeed used by some user I/O, but they can be re-purposed. If you have slower I/O that are not really affected by having the LED driver inputs connected, you could still use them.…
  • stefanrousseau
    0 stefanrousseau over 5 years ago

    AD3, AD4 and AD5 are indeed used by some user I/O, but they can be re-purposed.  If you have slower I/O that are not really affected by having the LED driver inputs connected, you could still use them.  The switch is of course more complicated.
    But if you look at the schematic, you will notice that the switch can be disconnected by removing R5.  Alternatively, all 3 signals can be disconnected by cutting through the traces in the middle of NTR10, NTR11 and NTR12.  These links have been placed on the PCB for this purpose.  If, after you have cut one of these, you decide to restore the original PCB connection again, you can solder-link or use a 0R resistor there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer