Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Cant run iperf (wifi) test from "Minized Getting started guide"
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 2260 views
  • Users 0 members are here
  • minized
Related

Cant run iperf (wifi) test from "Minized Getting started guide"

tmiller652
tmiller652 over 5 years ago

Hi There,

 

I've run all the steps in the "minized getting started guide" section 8 "WI-FI" and I can't get the  performance test to run when I issue the command '"perf3 -c 192.168.0.11" from my windows host computer. Note below that I can ping the device, but when I start the iperf server running on the minized and then issue the "iperf3 -c 192.168.0.11" from the windows command line, the error message is "unable to connect to server: Connection refused".  Has anyone seen this behavior or know how to correct it?

 

Best Regards,

Tom MIller

 

 

C:\Users\18054\Downloads\iperf-3.1.3-win64\iperf-3.1.3-win64>ping 192.168.0.11

 

Pinging 192.168.0.11 with 32 bytes of data:

Reply from 192.168.0.11: bytes=32 time=268ms TTL=64

Reply from 192.168.0.11: bytes=32 time=70ms TTL=64

Reply from 192.168.0.11: bytes=32 time=82ms TTL=64

Reply from 192.168.0.11: bytes=32 time=94ms TTL=64

 

Ping statistics for 192.168.0.11:

    Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),

Approximate round trip times in milli-seconds:

    Minimum = 70ms, Maximum = 268ms, Average = 128ms

 

 

C:\Users\18054\Downloads\iperf-3.1.3-win64\iperf-3.1.3-win64>iperf3 -c 192.168.0.11

iperf3: error - unable to connect to server: Connection refused

  • Sign in to reply
  • Cancel
Parents
  • tmiller652
    0 tmiller652 over 5 years ago

    Just a quick update; I can get the client and server sides of the test to connect now by specifying the port in addition to the address when launching the client:

     

    iperf3 -c 192.168.0.11 -p5001 -t10

     

    But the test still doesn't complete in the specified 10 seconds and only 14 bytes of data are transferred. I can complete the rest of the section 8 steps, including ping various websites and downloading a file via FTP, so it appears as if the WFI is working and I may just move on. But if anyone experiences this same sort of test failure and finds an answer I'd very much appreciate it if you could post a reply here.

     

    Best Regards,

    Tom Miller

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 5 years ago in reply to tmiller652

    Hi Tom,

     

    Does the Wi-Fi work for other things besides ping?

     

    I haven't tried iperf recently on MiniZed, but I have been using it on Ultra96-V2. I did not specify the port, but the iperf3 reported using Port 5201 on my Ultra96-V2. When I ran the Ultra96-V2 in client mode, I used the following commands:

      Windows  iperf3 -s -i 2 -1

      Ultra96-V2  iperf3 -c <ip address> -i 2 -t 20

     

    Which MiniZed build are you using?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 5 years ago in reply to tmiller652

    Hi Tom,

     

    Does the Wi-Fi work for other things besides ping?

     

    I haven't tried iperf recently on MiniZed, but I have been using it on Ultra96-V2. I did not specify the port, but the iperf3 reported using Port 5201 on my Ultra96-V2. When I ran the Ultra96-V2 in client mode, I used the following commands:

      Windows  iperf3 -s -i 2 -1

      Ultra96-V2  iperf3 -c <ip address> -i 2 -t 20

     

    Which MiniZed build are you using?

     

    Bryan