Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design reprogramming a minized from a USB drive using the uboot Zynq> prompt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • +1 person also asked this people also asked this
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 1429 views
  • Users 0 members are here
  • image.ub uboot minized
  • Report Bug
Related

reprogramming a minized from a USB drive using the uboot Zynq> prompt

GaryA
GaryA over 4 years ago

Hi,

I inadvertently removed the files from /run/media/mmcblk1d1 which contains the image.ub and smallboot.bin.

How do I get those files back into the eMMC from a USB drive?

I have read the "Restoring MiniZed to the Factory State" and it does not describe anything near what I require - it assumes that the device is up and running PetaLinux, which it is not.

Thanks for any and all help with this

NOTE: this problem was solved by invoking the following command from the Zynq> prompt

Zynq>run boot_qspi.

Once that command was run then the entire filesystem was available and I could copy the files back into the designated folder. YES!!!

I wish that information was in the "Restoring MiniZed to the Factory State" document.

  • Sign in to reply
  • Cancel

Top Replies

  • GaryA
    GaryA over 4 years ago +1 verified
    this problem was solved by invoking the following command from the Zynq> prompt Zynq>run boot_qspi. Once that command was run then the entire filesystem was available and I could copy the files back…
Parents
  • GaryA
    +1 GaryA over 4 years ago

    this problem was solved by invoking the following command from the Zynq> prompt

    Zynq>run boot_qspi.

    Once that command was run then the entire filesystem was available and I could copy the files back into the designated folder. YES!!!

    I wish that information was in the "Restoring MiniZed to the Factory State" document.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • GaryA
    +1 GaryA over 4 years ago

    this problem was solved by invoking the following command from the Zynq> prompt

    Zynq>run boot_qspi.

    Once that command was run then the entire filesystem was available and I could copy the files back into the designated folder. YES!!!

    I wish that information was in the "Restoring MiniZed to the Factory State" document.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer