Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed Sainsmart relay connection
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1888 views
  • Users 0 members are here
Related

MiniZed Sainsmart relay connection

tanderson
tanderson over 4 years ago

I am driving a Sainsmart 4 Relay Module from MiniZed.

Because it needs 5 volts, I connected JD-VCC to 5v on Arduino Shield of MiniZed.

VCC is connected to 3.3v VCC of MiniZed.

Ground is connected to ground.

IN4 of Sainsmart is connected to an output of MiniZed.

The relay allows a connected module to have its VCC connected/disconnected on K4 of Sainsmart.

All seems to be working well, but I am wondering if 5v of relay could draw too much power. I did not see any specs for 5v on the MiniZed HW users guide.

An alternative would be using an external 5v power supply (breadboard power supply), but so far, the setup appears to work.

I plan on doing some testing of the setup, and I would not want to jeopardize my MiniZed.

Regards,

Todd Anderson

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 4 years ago

    Hey Todd,

    Could you provide a simple diagram of what you are talking about? I think I follow but I don't want to make any assumptions. 5V on MiniZed through the Arduino is passed straight from Vin through a 0 ohm (0603) resistor. Your current capacity is theoretically limited by the current rating of that resistor, which is the lowest rated in the path. Double check the current draw on your relays and make sure it doesn't exceed the rating for a 0 ohm 0603, for reference Vishay says about 1.5A max - https://www.vishay.com/docs/31017/rcwp99.pdf

    R83 should be the limiting device image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tanderson
    0 tanderson over 4 years ago in reply to ctammann

    image

    This is what I ended up doing - I needed 5 volts for the JD-VCC, and I was not able to consistently bring it from MiniZed, so I used a separate power supply. SEL1 is used as IN4 input to control the normally open connections. Vcc is 3.3 volts. There is common ground. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tanderson
    0 tanderson over 4 years ago in reply to tanderson

    FWIW, I swapped out the Relay 4 Board for a single-relay board that runs on 3.3 volts. I did not require an external power supply, MiniZed Vcc worked just fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tanderson
    0 tanderson over 4 years ago in reply to tanderson

    FWIW, I swapped out the Relay 4 Board for a single-relay board that runs on 3.3 volts. I did not require an external power supply, MiniZed Vcc worked just fine.