Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Send data between two Minizeds.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 620 views
  • Users 0 members are here
Related

Send data between two Minizeds.

alisonfqc
alisonfqc over 7 years ago

Hello guys,

 

 

I am a beginner in using the Zynq device and I am trying to perform data transfer between two Minized boards. Could anyone point me some material so that I can have a basis on this subject.

  • Sign in to reply
  • Cancel

Top Replies

  • dcsoutherner
    dcsoutherner over 7 years ago +1
    Hi Alison, let's talk about the kind, frequency, volume and time requirements for transferring data between zed boards. The type of data (such as sensor readings, program execution commands, voice or video…
Parents
  • dcsoutherner
    dcsoutherner over 7 years ago

    Hi Alison, let's talk about the kind, frequency, volume and time requirements for transferring data between zed boards.

    The type of data (such as sensor readings, program execution commands, voice or video streams, etc) you want to send will help determine how the transfer is done.

    The volume, frequency and time requirements will also affect the method as well as the media.

    If you want to look into a fairly technical introduction to transferring data between zedboards, have a look at this 5 video series on youtube: https://www.youtube.com/watch?v=fBujI5d3DKM .  The creator of that series is well-known in the Xilinx community and it's worth a look.  In particular the 4th video will show how connections are made, but you should start with the first and see all 5.  Be aware that he is using different boards and the interfaces he discusses might not be the best fit to your needs, but you should be able to adapt what he demonstrates.

    Please reply and provide more details about your project.

    Good luck with it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dcsoutherner
    dcsoutherner over 7 years ago

    Hi Alison, let's talk about the kind, frequency, volume and time requirements for transferring data between zed boards.

    The type of data (such as sensor readings, program execution commands, voice or video streams, etc) you want to send will help determine how the transfer is done.

    The volume, frequency and time requirements will also affect the method as well as the media.

    If you want to look into a fairly technical introduction to transferring data between zedboards, have a look at this 5 video series on youtube: https://www.youtube.com/watch?v=fBujI5d3DKM .  The creator of that series is well-known in the Xilinx community and it's worth a look.  In particular the 4th video will show how connections are made, but you should start with the first and see all 5.  Be aware that he is using different boards and the interfaces he discusses might not be the best fit to your needs, but you should be able to adapt what he demonstrates.

    Please reply and provide more details about your project.

    Good luck with it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • alisonfqc
    alisonfqc over 7 years ago in reply to dcsoutherner

    dcsoutherner, thanks for the reply.

     

     

    About my project, I am performing the data acquisition through an accelerometer, data of 12 bits and the frequency of 100 kHz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dcsoutherner
    dcsoutherner over 7 years ago in reply to alisonfqc

    Hi Alison, I am assuming you can't attach the accelerometer directly to the Zync device where the data is needed or dual-porting it to multiple boards.

    There are several ways to transfer the data, beginning with a simple GPIO connection or wireless.  For more volume-intensive requirements you can consider I2C or at the extreme end CCIX.  All of these require programming beyond VHDL and Veriolog.